<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Max. speed CAN_clk in LPCXpresso IDE</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/Max-speed-CAN-clk/m-p/590210#M29003</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by luky on Thu Sep 01 23:56:35 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I have a LPCXpresso with the LPC11C24, but I have changed the Oscillator to 20MHz to run the Chip at 50MHz. Now I want to use the C_CAN Module (Baudrate 50k) and I have Problems to select the correct Register values.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;What is the max. frequency (or recommended frequency) for the CAN-Module? All examples use 8MHz, but that won't work in my case.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Is there a chance to get 50k Baudrate with minmimal Tolerances with the 20MHz Crystal Oscillator or should I change it back to 12MHz?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 21:27:00 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T21:27:00Z</dc:date>
    <item>
      <title>Max. speed CAN_clk</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Max-speed-CAN-clk/m-p/590210#M29003</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by luky on Thu Sep 01 23:56:35 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I have a LPCXpresso with the LPC11C24, but I have changed the Oscillator to 20MHz to run the Chip at 50MHz. Now I want to use the C_CAN Module (Baudrate 50k) and I have Problems to select the correct Register values.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;What is the max. frequency (or recommended frequency) for the CAN-Module? All examples use 8MHz, but that won't work in my case.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Is there a chance to get 50k Baudrate with minmimal Tolerances with the 20MHz Crystal Oscillator or should I change it back to 12MHz?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 21:27:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Max-speed-CAN-clk/m-p/590210#M29003</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T21:27:00Z</dc:date>
    </item>
  </channel>
</rss>