<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDEのトピックdebugging bootloader hardware fault</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/debugging-bootloader-hardware-fault/m-p/589293#M28568</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by gudushen on Thu Sep 01 13:13:06 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi, I have a firmware that jumps to a bootloader running on LPC1754. Now this works correctly for the lpcxpresso development board (lpc1769). However with the same software and bootloader it does not work with the LPC1754. It generates a hardware fault on entry to the bootloader at push(r3,lr). Any ideas why this only happens on the 1754 or what I can do to debug this would be greatly appreciated. Thanks&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 21:27:04 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T21:27:04Z</dc:date>
    <item>
      <title>debugging bootloader hardware fault</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/debugging-bootloader-hardware-fault/m-p/589293#M28568</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by gudushen on Thu Sep 01 13:13:06 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi, I have a firmware that jumps to a bootloader running on LPC1754. Now this works correctly for the lpcxpresso development board (lpc1769). However with the same software and bootloader it does not work with the LPC1754. It generates a hardware fault on entry to the bootloader at push(r3,lr). Any ideas why this only happens on the 1754 or what I can do to debug this would be greatly appreciated. Thanks&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 21:27:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/debugging-bootloader-hardware-fault/m-p/589293#M28568</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T21:27:04Z</dc:date>
    </item>
    <item>
      <title>Re: debugging bootloader hardware fault</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/debugging-bootloader-hardware-fault/m-p/589294#M28569</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by gudushen on Fri Sep 02 06:06:57 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I found the problem. Seems like this only happens with LPCXpresso 4.0.x, using 3.6.x, I was able to flash to the correct address&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 21:27:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/debugging-bootloader-hardware-fault/m-p/589294#M28569</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T21:27:05Z</dc:date>
    </item>
  </channel>
</rss>