<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Unable to enter debug in LPCXpresso IDE</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/Unable-to-enter-debug/m-p/589182#M28506</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by NXP_USA on Tue Feb 23 01:33:35 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: richas&lt;/STRONG&gt;&lt;BR /&gt;In playing with the settings I seem to have created two LPCxpresso boards that will no&amp;nbsp; longer enter debug mode.&lt;BR /&gt;When I try to connect I get a "Invalid ACK returned from DP access".&lt;BR /&gt;&lt;BR /&gt;I try a co-workers board and it works.&lt;BR /&gt;&lt;BR /&gt;I had been playing with the settings in the system_LPC11xx.c file in the CMSIS project, namely those pertaining to the PLL and clock source.&lt;BR /&gt;&lt;BR /&gt;Any way to recover these boards or are they bricks?&lt;BR /&gt;&lt;BR /&gt;In the process of trying to get them to work I reinstalled the IDE.&amp;nbsp; :P&lt;BR /&gt;&lt;BR /&gt;Rich&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Tie the ISP pin (P0.1) to ground. Upon reset/power-up, this will cause the board to enter ISP mode instead of running the user flash code. At this point the board can be reprogrammed by ISP through the UART, or the SWD port (driven by LPC-LINK) can take control of the board while it is running the ISP firmware and erase/program the flash memory.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;-NXP&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jun 2016 00:13:05 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-16T00:13:05Z</dc:date>
    <item>
      <title>Unable to enter debug</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Unable-to-enter-debug/m-p/589178#M28502</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by richas on Thu Feb 18 13:20:39 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;In playing with the settings I seem to have created two LPCxpresso boards that will no&amp;nbsp; longer enter debug mode.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;When I try to connect I get a "Invalid ACK returned from DP access".&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I try a co-workers board and it works.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I had been playing with the settings in the system_LPC11xx.c file in the CMSIS project, namely those pertaining to the PLL and clock source.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Any way to recover these boards or are they bricks?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;In the process of trying to get them to work I reinstalled the IDE.&amp;nbsp; :P&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Rich&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:13:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Unable-to-enter-debug/m-p/589178#M28502</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T00:13:02Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to enter debug</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Unable-to-enter-debug/m-p/589179#M28503</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by richas on Thu Feb 18 16:06:20 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I built up an rs232 converter circuit and buttons on P0.1 and reset.&amp;nbsp; Using Flashmagic I was able to erase the micro and now debug works.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Rich&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:13:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Unable-to-enter-debug/m-p/589179#M28503</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T00:13:03Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to enter debug</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Unable-to-enter-debug/m-p/589180#M28504</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by noritan_org on Thu Feb 18 21:47:59 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Is the FlashMagic available when the RESET pin is configured as GPIO ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I wonder how the LPCXpresso board works when P0_0 is configured as GPIO.&amp;nbsp; I can try it but I didn't because I am afraid that the LPCXpresso board may be unusable.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Does anyone try that configuration ?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:13:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Unable-to-enter-debug/m-p/589180#M28504</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T00:13:04Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to enter debug</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Unable-to-enter-debug/m-p/589181#M28505</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by rkiryanov on Fri Feb 19 00:16:10 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: noritan_org&lt;/STRONG&gt;&lt;BR /&gt;I am afraid&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Tie ISP pin to GND and don't worry. Anyway, NXP did a bad thing, RESET pin must be non-configurable.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:13:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Unable-to-enter-debug/m-p/589181#M28505</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T00:13:05Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to enter debug</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Unable-to-enter-debug/m-p/589182#M28506</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by NXP_USA on Tue Feb 23 01:33:35 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: richas&lt;/STRONG&gt;&lt;BR /&gt;In playing with the settings I seem to have created two LPCxpresso boards that will no&amp;nbsp; longer enter debug mode.&lt;BR /&gt;When I try to connect I get a "Invalid ACK returned from DP access".&lt;BR /&gt;&lt;BR /&gt;I try a co-workers board and it works.&lt;BR /&gt;&lt;BR /&gt;I had been playing with the settings in the system_LPC11xx.c file in the CMSIS project, namely those pertaining to the PLL and clock source.&lt;BR /&gt;&lt;BR /&gt;Any way to recover these boards or are they bricks?&lt;BR /&gt;&lt;BR /&gt;In the process of trying to get them to work I reinstalled the IDE.&amp;nbsp; :P&lt;BR /&gt;&lt;BR /&gt;Rich&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Tie the ISP pin (P0.1) to ground. Upon reset/power-up, this will cause the board to enter ISP mode instead of running the user flash code. At this point the board can be reprogrammed by ISP through the UART, or the SWD port (driven by LPC-LINK) can take control of the board while it is running the ISP firmware and erase/program the flash memory.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;-NXP&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:13:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Unable-to-enter-debug/m-p/589182#M28506</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T00:13:05Z</dc:date>
    </item>
  </channel>
</rss>