<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LPC1778 SPI Pullups or Not? in LPCXpresso IDE</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1778-SPI-Pullups-or-Not/m-p/532037#M2824</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by MikeSimmonds on Sun Jul 29 15:49:32 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;[FONT=Tahoma][SIZE=2]However, I nearly forgot the important part of the question (which is not addressed in the thread referenced).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Can I use the on-chip pullup rather than adding an external resistor?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;And at reset, the pin will be configured as an input with pullup by default.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;In general, will internal pullups work or are they not enabled for outputs?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Cheers, Mike[/SIZE][/FONT][FONT=Tahoma][SIZE=2]&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;[/SIZE][/FONT]&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jun 2016 01:39:33 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-16T01:39:33Z</dc:date>
    <item>
      <title>LPC1778 SPI Pullups or Not?</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1778-SPI-Pullups-or-Not/m-p/532034#M2821</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by MikeSimmonds on Sun Jul 29 14:58:17 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;[FONT=Tahoma][SIZE=2]When I configure pins for SPI funtionality can I (and should I!) set the SPI_CS to have its pullup enabled?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;What about the clock and data lines?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I've look at various manufacturer's datasheets for SPI devices; none seem to show pullups.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;However, At least one schematic I downloaded *does* have a pullup on the CS line.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;What's the best practice?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards, Mike :confused:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;[/SIZE][/FONT]&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 01:39:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1778-SPI-Pullups-or-Not/m-p/532034#M2821</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T01:39:31Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1778 SPI Pullups or Not?</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1778-SPI-Pullups-or-Not/m-p/532035#M2822</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Ex-Zero on Sun Jul 29 15:30:26 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Discussed here already:&amp;nbsp; &lt;/SPAN&gt;&lt;A href="http://"&gt;http://knowledgebase.nxp.com/showthread.php?t=2648&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;My favorite: CS pullup :rolleyes:&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 01:39:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1778-SPI-Pullups-or-Not/m-p/532035#M2822</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T01:39:32Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1778 SPI Pullups or Not?</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1778-SPI-Pullups-or-Not/m-p/532036#M2823</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by MikeSimmonds on Sun Jul 29 15:38:55 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;[FONT=Tahoma][SIZE=2]Thanks for the heads up.[/SIZE][/FONT] :)&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 01:39:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1778-SPI-Pullups-or-Not/m-p/532036#M2823</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T01:39:32Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1778 SPI Pullups or Not?</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1778-SPI-Pullups-or-Not/m-p/532037#M2824</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by MikeSimmonds on Sun Jul 29 15:49:32 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;[FONT=Tahoma][SIZE=2]However, I nearly forgot the important part of the question (which is not addressed in the thread referenced).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Can I use the on-chip pullup rather than adding an external resistor?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;And at reset, the pin will be configured as an input with pullup by default.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;In general, will internal pullups work or are they not enabled for outputs?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Cheers, Mike[/SIZE][/FONT][FONT=Tahoma][SIZE=2]&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;[/SIZE][/FONT]&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 01:39:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1778-SPI-Pullups-or-Not/m-p/532037#M2824</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T01:39:33Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1778 SPI Pullups or Not?</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1778-SPI-Pullups-or-Not/m-p/532038#M2825</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Ex-Zero on Sun Jul 29 17:49:19 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;As 'Fig 12 I/O configurations' of UM10470 shows, inputs use weak pullups. To avoid unintended CS activation (until your SPI setup is switching your CS to output) an external strong (10k) pullup is useful. So old-fashioned engineers add this pullup although almost all circuits work without it ;)&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 01:39:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1778-SPI-Pullups-or-Not/m-p/532038#M2825</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T01:39:33Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1778 SPI Pullups or Not?</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1778-SPI-Pullups-or-Not/m-p/532039#M2826</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by MikeSimmonds on Mon Jul 30 01:53:52 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;[FONT=Tahoma][SIZE=2]Thanks for that&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I am a firmware guy trying to talk to my hardware guy.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[/SIZE][/FONT]&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 01:39:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1778-SPI-Pullups-or-Not/m-p/532039#M2826</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T01:39:34Z</dc:date>
    </item>
  </channel>
</rss>