<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Who is using the USB Bootloader with MAC OS-X ? in LPCXpresso IDE</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/Who-is-using-the-USB-Bootloader-with-MAC-OS-X/m-p/587933#M27896</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by TheFallGuy on Sat Oct 29 09:08:47 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I don't know whether this trick will work for USB drives, but might be worth a look&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;A href="http://"&gt;http://osxdaily.com/2010/02/03/how-to-prevent-ds_store-file-creation/&lt;/A&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 21:28:46 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T21:28:46Z</dc:date>
    <item>
      <title>Who is using the USB Bootloader with MAC OS-X ?</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Who-is-using-the-USB-Bootloader-with-MAC-OS-X/m-p/587926#M27889</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Rob65 on Sun Aug 28 01:25:51 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I was wondering if there are more users out there with an Apple using the USBBootloader.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;As can be read in &lt;/SPAN&gt;&lt;A href="http://http://knowledgebase.nxp.com/showthread.php?t=2304"&gt;this thread&lt;/A&gt;&lt;SPAN&gt; DEGoodmanWilson is having problems downloading an image into the Flash using OS-X.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I then just realized that for one of my products I am confronted with a group of users that only work on MAC OS-X (I've talked to a number of photographers and some of them even don't own a PC)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;So it would be nice to know if there are other users that have similar problems with OS-X.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards,[INDENT]Rob&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[/INDENT]&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 21:28:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Who-is-using-the-USB-Bootloader-with-MAC-OS-X/m-p/587926#M27889</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T21:28:42Z</dc:date>
    </item>
    <item>
      <title>Re: Who is using the USB Bootloader with MAC OS-X ?</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Who-is-using-the-USB-Bootloader-with-MAC-OS-X/m-p/587927#M27890</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by kendwyer on Mon Aug 29 04:33:54 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I believe that this is discussed in the following AN:&lt;/SPAN&gt;&lt;BR /&gt;&lt;A href="http://"&gt;http://ics.nxp.com/support/documents/microcontrollers/zip/an10986.zip&lt;/A&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 21:28:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Who-is-using-the-USB-Bootloader-with-MAC-OS-X/m-p/587927#M27890</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T21:28:43Z</dc:date>
    </item>
    <item>
      <title>Re: Who is using the USB Bootloader with MAC OS-X ?</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Who-is-using-the-USB-Bootloader-with-MAC-OS-X/m-p/587928#M27891</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Rob65 on Mon Aug 29 23:32:47 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Ken,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I forgot to mention ... I was talking about the usb_bootloader for the lpc17xx series.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;that Application Note tells how to do automatic detection of the device and program the lpc13xx device with the ROM based USB bootloader - sadly the 1300 is the only series having this option built in ...&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;But the application note only talks about automatic detection and firmware update using a special tool. The thing is that when using the standard file manager in OS-X (Finder) the device is not programmed correctly (at least, DEGoodmanWilson was not able to do so). Command line programming seems to work.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have (will have) a base of users who are photographers. I found that a number of them are non-technical, they do know PhotoShop better than anyone else I know. They are also able to copy a file from one location to the other - but don't ask them to install special software ... &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;So I will be relying on the possibility to update software using a standard disk interface, other options are SD card or USB memory stick.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Rob&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 21:28:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Who-is-using-the-USB-Bootloader-with-MAC-OS-X/m-p/587928#M27891</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T21:28:43Z</dc:date>
    </item>
    <item>
      <title>Re: Who is using the USB Bootloader with MAC OS-X ?</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Who-is-using-the-USB-Bootloader-with-MAC-OS-X/m-p/587929#M27892</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by mhjerde on Tue Aug 30 12:22:34 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi Rob&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm also working on a device for photographers, using the lpc17xx series and hoping to support firmware upgrades on OS X :-) You are right that all photogs uses Macs.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I've yet to dive in to the details of the usb bootloader. Maybe it is time to get started.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 21:28:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Who-is-using-the-USB-Bootloader-with-MAC-OS-X/m-p/587929#M27892</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T21:28:44Z</dc:date>
    </item>
    <item>
      <title>Re: Who is using the USB Bootloader with MAC OS-X ?</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Who-is-using-the-USB-Bootloader-with-MAC-OS-X/m-p/587930#M27893</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Rob65 on Tue Aug 30 22:39:50 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: mhjerde&lt;/STRONG&gt;&lt;BR /&gt;I've yet to dive in to the details of the usb bootloader. Maybe it is time to get started.&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Actually, mine is kind of finished - but my customer/distributor of the product stopped his business ... &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;You can always use the application that Ken mentioned - that should work.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The thing is that there seems to be a difference in the way Finder and the command line write to the USB bootloader. Bootloader does not like this and messes up the code ...&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Command line works (according to DE) but then you do need to provide a proper manual on how to do this.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Rob&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 21:28:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Who-is-using-the-USB-Bootloader-with-MAC-OS-X/m-p/587930#M27893</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T21:28:44Z</dc:date>
    </item>
    <item>
      <title>Re: Who is using the USB Bootloader with MAC OS-X ?</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Who-is-using-the-USB-Bootloader-with-MAC-OS-X/m-p/587931#M27894</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by mhjerde on Wed Aug 31 11:09:23 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: Rob65&lt;/STRONG&gt;&lt;BR /&gt;Actually, mine is kind of finished - but my customer/distributor of the product stopped his business ... &lt;BR /&gt;&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Well, that is a bummer. So your work is just being shelved?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I've done a bit of testing on the Mac. It looks like the Mac tries to write additional data when copying the file. This is probably to store the resource fork. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I got an 'not enough space' error. Copying with the cp command did not work either for this test.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 21:28:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Who-is-using-the-USB-Bootloader-with-MAC-OS-X/m-p/587931#M27894</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T21:28:45Z</dc:date>
    </item>
    <item>
      <title>Re: Who is using the USB Bootloader with MAC OS-X ?</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Who-is-using-the-USB-Bootloader-with-MAC-OS-X/m-p/587932#M27895</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by DEGoodmanWilson on Sat Oct 29 05:57:04 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: mhjerde&lt;/STRONG&gt;&lt;BR /&gt;Well, that is a bummer. So your work is just being shelved?&lt;BR /&gt;&lt;BR /&gt;I've done a bit of testing on the Mac. It looks like the Mac tries to write additional data when copying the file. This is probably to store the resource fork. &lt;BR /&gt;I got an 'not enough space' error. Copying with the cp command did not work either for this test.&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Of course, I didn't think of the extra files that OS X tries to create. That might very well be the culprit.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;That said, I've been using the command line 'cp' method consistently since I first mentioned this issue. I agree that it is no good for end-users, but it at least permits me to get code on the board from my Mac! I wonder why it isn't working for you?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 21:28:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Who-is-using-the-USB-Bootloader-with-MAC-OS-X/m-p/587932#M27895</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T21:28:46Z</dc:date>
    </item>
    <item>
      <title>Re: Who is using the USB Bootloader with MAC OS-X ?</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Who-is-using-the-USB-Bootloader-with-MAC-OS-X/m-p/587933#M27896</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by TheFallGuy on Sat Oct 29 09:08:47 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I don't know whether this trick will work for USB drives, but might be worth a look&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;A href="http://"&gt;http://osxdaily.com/2010/02/03/how-to-prevent-ds_store-file-creation/&lt;/A&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 21:28:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Who-is-using-the-USB-Bootloader-with-MAC-OS-X/m-p/587933#M27896</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T21:28:46Z</dc:date>
    </item>
    <item>
      <title>Re: Who is using the USB Bootloader with MAC OS-X ?</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Who-is-using-the-USB-Bootloader-with-MAC-OS-X/m-p/587934#M27897</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by mhjerde on Thu Dec 15 10:14:41 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Has anyone made any progress on getting firmware updating to work on a Mac?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;There seems to be some workarounds like using command line tools to copy the file or disable .DS_Store file creation, but that won't fly with end users.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;If the problem is that the Mac attempts to store the resource fork in a subdirectory, maybe it would be possible to circumvent this by implementing dummy commands in the bootloader?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 21:28:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Who-is-using-the-USB-Bootloader-with-MAC-OS-X/m-p/587934#M27897</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T21:28:47Z</dc:date>
    </item>
  </channel>
</rss>