<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDEのトピックRe: Adding emWin do LPC project and C++ application</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/Adding-emWin-do-LPC-project-and-C-application/m-p/587339#M27609</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by NXP_Support on Thu Apr 09 14:09:00 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello Littlejohh,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I see that NXP does not have an easy to find overview of how to add emWin to a project - sorry about that!&amp;nbsp; &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Please download the LPCOpen package for Keil MCB 1857 or Keil MCB 4357 [These are the only boards that has LCD built into and will support emWin without add on LCD modules] and import “emWin [emWin library placeholder project]”, “emwin_hello_world [Hello World example]” and “emwin_with_touch [Touch Screen example]” along with the board and chip libraries. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Inside the emWin project there is a “installation.txt” file that explains how to install the emwin libraries into the project area.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Best regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;-NXP Support&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jun 2016 00:06:38 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-16T00:06:38Z</dc:date>
    <item>
      <title>Adding emWin do LPC project and C++ application</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Adding-emWin-do-LPC-project-and-C-application/m-p/587338#M27608</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by littlejohn on Thu Apr 09 06:26:47 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have problem with adding emWin library do my LPCXpresso project. I have read emWin documentation, but I still don't know.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Please give mi advice in order what I should to do. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I would like to add emWin to my project, create window and in this window show applicaion wrtitten in C++.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Then done application upload do Cortex M4. From what I can start?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Best regards :)&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:06:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Adding-emWin-do-LPC-project-and-C-application/m-p/587338#M27608</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T00:06:37Z</dc:date>
    </item>
    <item>
      <title>Re: Adding emWin do LPC project and C++ application</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Adding-emWin-do-LPC-project-and-C-application/m-p/587339#M27609</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by NXP_Support on Thu Apr 09 14:09:00 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello Littlejohh,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I see that NXP does not have an easy to find overview of how to add emWin to a project - sorry about that!&amp;nbsp; &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Please download the LPCOpen package for Keil MCB 1857 or Keil MCB 4357 [These are the only boards that has LCD built into and will support emWin without add on LCD modules] and import “emWin [emWin library placeholder project]”, “emwin_hello_world [Hello World example]” and “emwin_with_touch [Touch Screen example]” along with the board and chip libraries. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Inside the emWin project there is a “installation.txt” file that explains how to install the emwin libraries into the project area.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Best regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;-NXP Support&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:06:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Adding-emWin-do-LPC-project-and-C-application/m-p/587339#M27609</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T00:06:38Z</dc:date>
    </item>
  </channel>
</rss>