<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDE中的主题 Re: Easyweb with FreeRTOS on LPC1769</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/Easyweb-with-FreeRTOS-on-LPC1769/m-p/586265#M27115</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by FlySnake on Thu Dec 06 02:13:07 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: kvanderkamp&lt;/STRONG&gt;&lt;BR /&gt;For a project I'm trying to combine TCP funcitonality with multiple thread support, specifically by combining easyweb with the FreeRTOS example code. Somehow if I add a breakpoint in the Init_EthMAC function just after it sets the PHY to autonegotiation link speed, the code runs well and I'm able to access the webserver. However if I remove the breakpoint it will throw a HardFault.&lt;BR /&gt;&lt;BR /&gt;Does anyone have a suggestion how to fix this, or even an alternative way of adding IP functionality to FreeRTOS?&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;A href="http://"&gt;http://www.freertos.org/FreeRTOS-Plus/FreeRTOS_Plus_IO/Demo_Applications/LPCXpresso_LPC1769/NXP_LPC1769_Demo_Description.shtml&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;A href="http://"&gt;https://bitbucket.org/antlabs_dev/lpc176x_freertos_lwip_skeleton&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Easyweb is too easy for production&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jun 2016 01:22:25 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-16T01:22:25Z</dc:date>
    <item>
      <title>Easyweb with FreeRTOS on LPC1769</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Easyweb-with-FreeRTOS-on-LPC1769/m-p/586264#M27114</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by kvanderkamp on Wed Dec 05 18:36:22 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;For a project I'm trying to combine TCP funcitonality with multiple thread support, specifically by combining easyweb with the FreeRTOS example code. Somehow if I add a breakpoint in the Init_EthMAC function just after it sets the PHY to autonegotiation link speed, the code runs well and I'm able to access the webserver. However if I remove the breakpoint it will throw a HardFault.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Does anyone have a suggestion how to fix this, or even an alternative way of adding IP functionality to FreeRTOS?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 01:22:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Easyweb-with-FreeRTOS-on-LPC1769/m-p/586264#M27114</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T01:22:23Z</dc:date>
    </item>
    <item>
      <title>Re: Easyweb with FreeRTOS on LPC1769</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Easyweb-with-FreeRTOS-on-LPC1769/m-p/586265#M27115</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by FlySnake on Thu Dec 06 02:13:07 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: kvanderkamp&lt;/STRONG&gt;&lt;BR /&gt;For a project I'm trying to combine TCP funcitonality with multiple thread support, specifically by combining easyweb with the FreeRTOS example code. Somehow if I add a breakpoint in the Init_EthMAC function just after it sets the PHY to autonegotiation link speed, the code runs well and I'm able to access the webserver. However if I remove the breakpoint it will throw a HardFault.&lt;BR /&gt;&lt;BR /&gt;Does anyone have a suggestion how to fix this, or even an alternative way of adding IP functionality to FreeRTOS?&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;A href="http://"&gt;http://www.freertos.org/FreeRTOS-Plus/FreeRTOS_Plus_IO/Demo_Applications/LPCXpresso_LPC1769/NXP_LPC1769_Demo_Description.shtml&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;A href="http://"&gt;https://bitbucket.org/antlabs_dev/lpc176x_freertos_lwip_skeleton&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Easyweb is too easy for production&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 01:22:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Easyweb-with-FreeRTOS-on-LPC1769/m-p/586265#M27115</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T01:22:25Z</dc:date>
    </item>
  </channel>
</rss>