<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDEのトピックRe: LPC1769 timer change</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1769-timer-change/m-p/531675#M2619</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Polux rsv on Sat Jul 14 15:12:51 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;RTFM. :D&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;There is 1 pwm, but with 6 outputs. And each timer could also generate several pwm.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Angelo&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jun 2016 01:36:06 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-16T01:36:06Z</dc:date>
    <item>
      <title>LPC1769 timer change</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1769-timer-change/m-p/531674#M2618</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by timer on Sat Jul 14 08:24:57 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I try to use the timer for a Delta-Modulation to drive a Motor-Controller.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;As the LPC has only 1 PWM I can't use it because I need four different frequencys.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I implement 1 Timer and all works fine with a constant frequency, but if I change it up to a sensor value suddenly (but not immediately, so I can change the speed of the motor) the Pulse is away.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Up to the debugger nothing change but the IR:MR0I is constant 0. The TC and PC are still counting but the interrupt routine is not anymore entering.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Have anyone an idea what this could cause?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Are you need my code?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks, Tim&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;EDIT:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I found a solution. Everytime I&amp;nbsp; change the frequency I reset, init and enable the timer.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Maybe this help someone else.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 01:36:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1769-timer-change/m-p/531674#M2618</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T01:36:05Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1769 timer change</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1769-timer-change/m-p/531675#M2619</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Polux rsv on Sat Jul 14 15:12:51 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;RTFM. :D&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;There is 1 pwm, but with 6 outputs. And each timer could also generate several pwm.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Angelo&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 01:36:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1769-timer-change/m-p/531675#M2619</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T01:36:06Z</dc:date>
    </item>
  </channel>
</rss>