<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDE中的主题 lpc1769 demo code</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/lpc1769-demo-code/m-p/583157#M25745</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by iantycoon on Sun Nov 06 18:52:33 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;may i know if anyone has the demo code which comes tgt with the lpc1769? the function it has are as follows:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[SIZE=3] &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;3 out of the 16 LEDs will always be lit and by tilting the board the LEDs that are lit will change (as a moving) bar. The way you move the board (in y-axis) will change the direction and speed of this bar. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The joystick can be used to draw on the OLED display. It is like moving a pen you never lift from the paper. By using the center key on the joystick the display is cleared. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Rotating the rotary switch will change which digit (0 to 9) is shown on the 7-segment display. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Pressing the SW3 button will start playing a melody. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Turning the trim potentiometer will turn on/off the RGB LEDs &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I lost mine. appreciate if anyone can upload it. thanks&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[/SIZE]&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 22:45:52 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T22:45:52Z</dc:date>
    <item>
      <title>lpc1769 demo code</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/lpc1769-demo-code/m-p/583157#M25745</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by iantycoon on Sun Nov 06 18:52:33 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;may i know if anyone has the demo code which comes tgt with the lpc1769? the function it has are as follows:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[SIZE=3] &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;3 out of the 16 LEDs will always be lit and by tilting the board the LEDs that are lit will change (as a moving) bar. The way you move the board (in y-axis) will change the direction and speed of this bar. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The joystick can be used to draw on the OLED display. It is like moving a pen you never lift from the paper. By using the center key on the joystick the display is cleared. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Rotating the rotary switch will change which digit (0 to 9) is shown on the 7-segment display. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Pressing the SW3 button will start playing a melody. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Turning the trim potentiometer will turn on/off the RGB LEDs &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I lost mine. appreciate if anyone can upload it. thanks&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[/SIZE]&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:45:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/lpc1769-demo-code/m-p/583157#M25745</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:45:52Z</dc:date>
    </item>
    <item>
      <title>Re: lpc1769 demo code</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/lpc1769-demo-code/m-p/583158#M25746</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by atomicdog on Sun Nov 06 20:15:26 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Did you check the NXP website?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:45:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/lpc1769-demo-code/m-p/583158#M25746</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:45:53Z</dc:date>
    </item>
  </channel>
</rss>