<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDEのトピックIAP RAM Requirements?</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/IAP-RAM-Requirements/m-p/527065#M257</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by scs on Wed Jan 25 12:06:03 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;The LPC17XX IAP built-in flash programming functions use 32 bytes in the "top portion of the on-chip RAM". But it is not clear which RAM, the normal RamLoc32 or the less used RamAHB32 second bank of RAM. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;If IAP uses the normal RamLoc32, then I should probably reserve 32 decimal bytes at the top of RAM in the CodeRed IDE, changing the MPU Linker Target "Stack offset" from 0 to 32.&amp;nbsp; But if IAP uses RamAHB32 then Stack offset 0 would be ok.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Does anyone know whether "Stack offset" 32 is recommended when my code uses IAP functions?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jun 2016 02:53:45 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-16T02:53:45Z</dc:date>
    <item>
      <title>IAP RAM Requirements?</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/IAP-RAM-Requirements/m-p/527065#M257</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by scs on Wed Jan 25 12:06:03 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;The LPC17XX IAP built-in flash programming functions use 32 bytes in the "top portion of the on-chip RAM". But it is not clear which RAM, the normal RamLoc32 or the less used RamAHB32 second bank of RAM. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;If IAP uses the normal RamLoc32, then I should probably reserve 32 decimal bytes at the top of RAM in the CodeRed IDE, changing the MPU Linker Target "Stack offset" from 0 to 32.&amp;nbsp; But if IAP uses RamAHB32 then Stack offset 0 would be ok.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Does anyone know whether "Stack offset" 32 is recommended when my code uses IAP functions?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 02:53:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/IAP-RAM-Requirements/m-p/527065#M257</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T02:53:45Z</dc:date>
    </item>
    <item>
      <title>Re: IAP RAM Requirements?</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/IAP-RAM-Requirements/m-p/527066#M258</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by NXP_USA on Thu Jan 26 10:10:35 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi!&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;IAP uses the top 32-bytes of the local RAM (not the AHB RAM). There is an NXP application note that shows how to get IAP to work on the LPC176x_5x.&lt;/SPAN&gt;&lt;BR /&gt;&lt;A href="http://"&gt;http://www.nxp.com/documents/application_note/AN10866.pdf&lt;/A&gt;&lt;BR /&gt;&lt;A href="http://"&gt;http://www.nxp.com/documents/other/LPC1700_secondary_USB_bootloader.zip&lt;/A&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 02:53:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/IAP-RAM-Requirements/m-p/527066#M258</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T02:53:46Z</dc:date>
    </item>
  </channel>
</rss>