<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LPC1768 problem with pin P2.10 in LPCXpresso IDE</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1768-problem-with-pin-P2-10/m-p/582953#M25655</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Michal on Sat Jul 07 06:28:31 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I have soldered my LPC1768 on the board and the pin P2.10 is still on high level (3.3V). I checked the board and there is no mistake. I picked up new LPC1768 and I made connection test. The result is that P2.10 is connect to pin 96 (Vdd3.3V) and to pin P1.30. Is it ok? I can not use ISP bootloader becouse when I connect P2.10 to GND I have a short circuit:(&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jun 2016 02:34:59 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-16T02:34:59Z</dc:date>
    <item>
      <title>LPC1768 problem with pin P2.10</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1768-problem-with-pin-P2-10/m-p/582953#M25655</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Michal on Sat Jul 07 06:28:31 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I have soldered my LPC1768 on the board and the pin P2.10 is still on high level (3.3V). I checked the board and there is no mistake. I picked up new LPC1768 and I made connection test. The result is that P2.10 is connect to pin 96 (Vdd3.3V) and to pin P1.30. Is it ok? I can not use ISP bootloader becouse when I connect P2.10 to GND I have a short circuit:(&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 02:34:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1768-problem-with-pin-P2-10/m-p/582953#M25655</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T02:34:59Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1768 problem with pin P2.10</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1768-problem-with-pin-P2-10/m-p/582954#M25656</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Ex-Zero on Sat Jul 07 06:54:55 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I guess it is the first time you are soldering LPC1768 ;)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;What you are describing sounds like as you have mixed up pin1 :eek:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Described in &lt;/SPAN&gt;&lt;A href="http://"&gt;http://knowledgebase.nxp.com/showthread.php?p=14562&amp;amp;langid=1&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Picture: &lt;/SPAN&gt;&lt;A href="http://"&gt;http://flic.kr/p/bxSbea&lt;/A&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 02:35:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1768-problem-with-pin-P2-10/m-p/582954#M25656</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T02:35:00Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1768 problem with pin P2.10</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1768-problem-with-pin-P2-10/m-p/582955#M25657</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Luis Digital on Sat Jul 07 07:07:38 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;The first time, I too made the same mistake. lol&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 02:35:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1768-problem-with-pin-P2-10/m-p/582955#M25657</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T02:35:00Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1768 problem with pin P2.10</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1768-problem-with-pin-P2-10/m-p/582956#M25658</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Michal on Sat Jul 07 08:10:39 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I can not believe it! You are right :) Shame on my!&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 02:35:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1768-problem-with-pin-P2-10/m-p/582956#M25658</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T02:35:01Z</dc:date>
    </item>
  </channel>
</rss>