<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDE中的主题 Re: Newbie Question - GPIO pin allocation</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/Newbie-Question-GPIO-pin-allocation/m-p/531521#M2549</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Ex-Zero on Mon May 14 08:18:26 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;If you don't need this special timer functions (like match or capture) it's of course not necessary to enable them (and waste a pin) :)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Libraries are just libraries, you don't know if they do what you want. So don't trust them :mad: They often set or reset functions and surprise us :eek:&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jun 2016 00:18:22 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-16T00:18:22Z</dc:date>
    <item>
      <title>Newbie Question - GPIO pin allocation</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Newbie-Question-GPIO-pin-allocation/m-p/531520#M2548</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by a.unique.identifier on Mon May 14 06:57:03 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I've noticed many cases in which the libraries associated with an internal resource, such as the 32 bit timer, also set the appropriate GPIO pins accordingly (ex.: The NXP init_timer32 routine sets the pins for CAP0, MAT0, etc.). If I'm using the timer for a blocking delay or to cause an interrupt, I can use the CAP0, MAT0, etc. - or a subset of these pins - for other GPIO functions, correct? I tested this using these GPIO pins for something else and it seems to work fine. I wanted to make certain I wasn't missing some fine point.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;This is a general question, but specifically I'm using the LPC1343.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks!&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:18:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Newbie-Question-GPIO-pin-allocation/m-p/531520#M2548</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T00:18:21Z</dc:date>
    </item>
    <item>
      <title>Re: Newbie Question - GPIO pin allocation</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Newbie-Question-GPIO-pin-allocation/m-p/531521#M2549</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Ex-Zero on Mon May 14 08:18:26 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;If you don't need this special timer functions (like match or capture) it's of course not necessary to enable them (and waste a pin) :)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Libraries are just libraries, you don't know if they do what you want. So don't trust them :mad: They often set or reset functions and surprise us :eek:&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:18:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Newbie-Question-GPIO-pin-allocation/m-p/531521#M2549</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T00:18:22Z</dc:date>
    </item>
    <item>
      <title>Re: Newbie Question - GPIO pin allocation</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Newbie-Question-GPIO-pin-allocation/m-p/531522#M2550</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by a.unique.identifier on Mon May 14 09:57:27 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks for the confirmation!&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:18:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Newbie-Question-GPIO-pin-allocation/m-p/531522#M2550</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T00:18:22Z</dc:date>
    </item>
  </channel>
</rss>