<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDE中的主题 Re: Debug problem LPC1769 Linux</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/Debug-problem-LPC1769-Linux/m-p/582299#M25347</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by frame on Tue Jun 21 23:31:44 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I have the same problem with two machines, one Suse11.2-x64 and one on Suse 11.0&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;However, I come so far only if I start the IDE as root. As normal user, it fails initializing the lpc-link with a timeout message (it fails to download the LPCXpressoWin.enc, because of access rights issues for /dev/usb).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The same board work under Windows, so it' neither a hardware issue nor a problem&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;of a specific Suse release.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jun 2016 02:34:58 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-16T02:34:58Z</dc:date>
    <item>
      <title>Debug problem LPC1769 Linux</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Debug-problem-LPC1769-Linux/m-p/582296#M25344</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by FlySnake on Tue Jun 21 10:31:16 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi all!&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Please help me with a problem.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm trying to use LPCXpresso 1769 and Base Board from EmbeddedArtists. I've installed LPCXpresso IDE v3.8.3 on Linux openSUSE 11.2 (kernel 2.6.31.14-0.8-default). It runs OK, but I cannot debug any sample project. When I click on debug, it gives me error message:&lt;/SPAN&gt;&lt;BR /&gt;&lt;TABLE border="1"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD bgcolor="#cacaca"&gt; &lt;PRE&gt;Error launching Debug/demo.axf
putpkt: write failed: Broken pipe.:&lt;/PRE&gt; &lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;SPAN&gt;But, I can flash the MCU by selecting "Binary Utilities / Program flash..." from context menu and it will work. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;It looks like the known issue:&lt;/SPAN&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: &lt;/STRONG&gt;&lt;BR /&gt;LPCXpresso for Linux cannot connect to an RDB1768v2 board using the&amp;nbsp; built in debug connection unless the RDB1768v2 has been updated to the &lt;A href="http://http://support.code-red-tech.com/CodeRedWiki/RDB1768V2firmware" rel="nofollow noopener noreferrer" target="_blank"&gt;latest debug firmware.&lt;/A&gt; Note that updating the RDB1768v2 debug firmware is currently only possible under Windows. &lt;/SPAN&gt;&lt;HR /&gt;&lt;SPAN&gt;But I'm not sure because I use another board and slightly different chip.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 02:34:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Debug-problem-LPC1769-Linux/m-p/582296#M25344</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T02:34:56Z</dc:date>
    </item>
    <item>
      <title>Re: Debug problem LPC1769 Linux</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Debug-problem-LPC1769-Linux/m-p/582297#M25345</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Luis Digital on Tue Jun 21 11:43:45 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Try updating your OpenSuse first, and then &lt;/SPAN&gt;&lt;A href="http://http://knowledgebase.nxp.com/showthread.php?p=6837"&gt;see&lt;/A&gt;&lt;A href="http://http://knowledgebase.nxp.com/showthread.php?p=6837"&gt; &lt;/A&gt;&lt;A href="http://http://knowledgebase.nxp.com/showthread.php?p=6837"&gt;this thread&lt;/A&gt;&lt;SPAN&gt;.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 02:34:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Debug-problem-LPC1769-Linux/m-p/582297#M25345</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T02:34:57Z</dc:date>
    </item>
    <item>
      <title>Re: Debug problem LPC1769 Linux</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Debug-problem-LPC1769-Linux/m-p/582298#M25346</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by FlySnake on Tue Jun 21 12:32:16 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Just tried this on another PC with 11.4. Fail again, but now it said:&lt;/SPAN&gt;&lt;BR /&gt;&lt;TABLE border="1"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD bgcolor="#cacaca"&gt; &lt;PRE&gt;Error launching Debug/demo.axf
Remote communication error: connection reset by peer.:&lt;/PRE&gt; &lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;SPAN&gt;I still can flash the program, but not debug it as in the first case. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Of course I can try Ubuntu if this is 100% distro's problem, but it's more likely I'm doing something wrong, not OS.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 02:34:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Debug-problem-LPC1769-Linux/m-p/582298#M25346</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T02:34:58Z</dc:date>
    </item>
    <item>
      <title>Re: Debug problem LPC1769 Linux</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Debug-problem-LPC1769-Linux/m-p/582299#M25347</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by frame on Tue Jun 21 23:31:44 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I have the same problem with two machines, one Suse11.2-x64 and one on Suse 11.0&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;However, I come so far only if I start the IDE as root. As normal user, it fails initializing the lpc-link with a timeout message (it fails to download the LPCXpressoWin.enc, because of access rights issues for /dev/usb).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The same board work under Windows, so it' neither a hardware issue nor a problem&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;of a specific Suse release.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 02:34:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Debug-problem-LPC1769-Linux/m-p/582299#M25347</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T02:34:58Z</dc:date>
    </item>
  </channel>
</rss>