<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDEのトピックRe: LPC11C14 port pull-up resistor value ?</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC11C14-port-pull-up-resistor-value/m-p/531487#M2530</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by NXP_Europe on Sun Feb 19 03:00:46 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;[FONT=Arial]Hello DaveNadler,[/FONT]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[FONT=Arial]The pull-up and pull-down 'weaks' are not actual resistors. They are transistors configured as a current source.[/FONT]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[FONT=Arial]They are 'weak' current sources. For simplicity we call them resistors.[/FONT] &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[FONT=Arial]What kind of ESD suppression do you have in mind?[/FONT]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[FONT=Arial]Otherwise, I would suggest, if critical, not to use the 'weak' resistor part and to use external resistors.[/FONT]&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jun 2016 02:55:34 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-16T02:55:34Z</dc:date>
    <item>
      <title>LPC11C14 port pull-up resistor value ?</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC11C14-port-pull-up-resistor-value/m-p/531485#M2528</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by DaveNadler on Sat Feb 18 15:30:06 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;[FONT=Arial]Sorry if I'm being dense, but I cannot find the range of values for the built-in pull-up or pull-down resistors on GPIO ports. All the diagrams (user manual and datasheet) just say "weak". I need to know the actual range of values.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks in advance, Best Regards, Dave&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;PS: This to ensure external ESD-suppression components are sized such that the port still works as an input...&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;PPS: Input current graph seems to imply min 50ua for Vin &amp;lt; 1v, or equivalent of ~66k for 3.3v supply ? Is this the only spec ? Graph is "Fig 16. Typical pull-up current Ipu versus input voltage VI"&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[/FONT]&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 02:55:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC11C14-port-pull-up-resistor-value/m-p/531485#M2528</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T02:55:32Z</dc:date>
    </item>
    <item>
      <title>Re: LPC11C14 port pull-up resistor value ?</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC11C14-port-pull-up-resistor-value/m-p/531486#M2529</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by js-nxp on Sat Feb 18 19:17:23 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;The internal "weak" resistors are usually in the range of 30K-100K with [B]OTHER[/B] micros I work with. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I would suggest that you turn off the resistors if you have external ESD or other networks which can keep the pin at the require quiescent state.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 02:55:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC11C14-port-pull-up-resistor-value/m-p/531486#M2529</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T02:55:33Z</dc:date>
    </item>
    <item>
      <title>Re: LPC11C14 port pull-up resistor value ?</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC11C14-port-pull-up-resistor-value/m-p/531487#M2530</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by NXP_Europe on Sun Feb 19 03:00:46 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;[FONT=Arial]Hello DaveNadler,[/FONT]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[FONT=Arial]The pull-up and pull-down 'weaks' are not actual resistors. They are transistors configured as a current source.[/FONT]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[FONT=Arial]They are 'weak' current sources. For simplicity we call them resistors.[/FONT] &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[FONT=Arial]What kind of ESD suppression do you have in mind?[/FONT]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[FONT=Arial]Otherwise, I would suggest, if critical, not to use the 'weak' resistor part and to use external resistors.[/FONT]&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 02:55:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC11C14-port-pull-up-resistor-value/m-p/531487#M2530</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T02:55:34Z</dc:date>
    </item>
  </channel>
</rss>