<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic enquiry on delay functions in LPCXpresso IDE</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/enquiry-on-delay-functions/m-p/531444#M2496</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by jx1 on Tue Jun 25 22:58:39 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I am trying to modify the dali master program. I manage to dim the lights to 10%.How do I make a delay so that it will brighten to 100% after a while? The dali master.c file i got it from here &lt;/SPAN&gt;&lt;A href="http://http://www.lpcware.com/content/nxpfile/an11174-and-an11175-lpc11xxlpc13xx-dali-release-20"&gt;http://www.lpcware.com/content/nxpfile/an11174-and-an11175-lpc11xxlpc13xx-dali-release-20&lt;/A&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jun 2016 01:36:06 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-16T01:36:06Z</dc:date>
    <item>
      <title>enquiry on delay functions</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/enquiry-on-delay-functions/m-p/531444#M2496</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by jx1 on Tue Jun 25 22:58:39 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I am trying to modify the dali master program. I manage to dim the lights to 10%.How do I make a delay so that it will brighten to 100% after a while? The dali master.c file i got it from here &lt;/SPAN&gt;&lt;A href="http://http://www.lpcware.com/content/nxpfile/an11174-and-an11175-lpc11xxlpc13xx-dali-release-20"&gt;http://www.lpcware.com/content/nxpfile/an11174-and-an11175-lpc11xxlpc13xx-dali-release-20&lt;/A&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 01:36:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/enquiry-on-delay-functions/m-p/531444#M2496</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T01:36:06Z</dc:date>
    </item>
    <item>
      <title>Re: enquiry on delay functions</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/enquiry-on-delay-functions/m-p/531445#M2497</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by CodeRedSupport on Wed Jun 26 00:28:55 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Plenty of example code is available which uses delays - typically by using the Systick timer peripheral.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I suggest that you look at the examples supplied in LPCXpresso for the actual MCU that you are using.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;CodeRedSupport&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 01:36:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/enquiry-on-delay-functions/m-p/531445#M2497</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T01:36:07Z</dc:date>
    </item>
  </channel>
</rss>