<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDEのトピックnewlib with debuginfo</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/newlib-with-debuginfo/m-p/581258#M24877</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by lpcentric on Tue Sep 27 23:56:32 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Is the newlib c runtime available with debuginfo and source (particularly the semihosted one), so one can step through with the debugger? I know the newlib source is available, but that doesn't get it into a debuggable state on the lpcxpresso.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks!&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 23:59:46 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T23:59:46Z</dc:date>
    <item>
      <title>newlib with debuginfo</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/newlib-with-debuginfo/m-p/581258#M24877</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by lpcentric on Tue Sep 27 23:56:32 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Is the newlib c runtime available with debuginfo and source (particularly the semihosted one), so one can step through with the debugger? I know the newlib source is available, but that doesn't get it into a debuggable state on the lpcxpresso.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks!&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:59:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/newlib-with-debuginfo/m-p/581258#M24877</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:59:46Z</dc:date>
    </item>
    <item>
      <title>Re: newlib with debuginfo</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/newlib-with-debuginfo/m-p/581259#M24878</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by CodeRedSupport on Wed Sep 28 03:34:40 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;We don't provide source for the Redlib and Newlib C libraries with LPCXpresso, though, as you note, the sources for Newlib are freely available.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;We also don't provide source for the "semihosting stubs" that sit underneath the C libraries when you configure the tools to use semihosting. However these stubs basically implement the semihosting specification as originally defined by ARM.&amp;nbsp; You can find this in the &lt;/SPAN&gt;&lt;A href="http://http://infocenter.arm.com/help/index.jsp?topic=/com.arm.doc.dui0058d/CIHBDHFF.html"&gt;ARM Developer Suite (ADS) v1.2 Debug Target Guide, Chapter 5. Semihosting&lt;/A&gt;&lt;SPAN&gt;.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;If you can explain what you are actually trying to achieve, then we might be able to advise more directly.&amp;nbsp; For example, if you simply want to retarget the C library to use, say, a uart as the target for printf rather than the semihosting console within the debugger then this FAQ should help:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;A href="http://"&gt;http://support.code-red-tech.com/CodeRedWiki/UartPrintf&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;And more general information on the C library can be found in the other FAQs at:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;A href="http://"&gt;http://support.code-red-tech.com/CodeRedWiki/CodeRedFAQ#CLibrary&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;CodeRedSupport&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:59:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/newlib-with-debuginfo/m-p/581259#M24878</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:59:47Z</dc:date>
    </item>
  </channel>
</rss>