<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDEのトピックMulti-function pins on LPC1343</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/Multi-function-pins-on-LPC1343/m-p/580986#M24767</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by err on Mon Jun 21 21:26:23 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm using an LPC1343 and one of the digital GPIO outputs doesn't work.&amp;nbsp; We're not using the SPI or UART, but PORT0_8 doesn't seem to work like the other digital outputs that are on single function I/O pins.&amp;nbsp; It must be due to configuration, but I just don't seem to see any such configuration code in any of my documentation or sample programs.&amp;nbsp; Any pointers would be greatly appreciated.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 22:38:15 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T22:38:15Z</dc:date>
    <item>
      <title>Multi-function pins on LPC1343</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Multi-function-pins-on-LPC1343/m-p/580986#M24767</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by err on Mon Jun 21 21:26:23 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm using an LPC1343 and one of the digital GPIO outputs doesn't work.&amp;nbsp; We're not using the SPI or UART, but PORT0_8 doesn't seem to work like the other digital outputs that are on single function I/O pins.&amp;nbsp; It must be due to configuration, but I just don't seem to see any such configuration code in any of my documentation or sample programs.&amp;nbsp; Any pointers would be greatly appreciated.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:38:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Multi-function-pins-on-LPC1343/m-p/580986#M24767</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:38:15Z</dc:date>
    </item>
    <item>
      <title>Re: Multi-function pins on LPC1343</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Multi-function-pins-on-LPC1343/m-p/580987#M24768</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by err on Tue Jun 22 11:58:34 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Found the problem. Using timer16_0, the init call configures this pin as a timer input....&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Commented line out, now it works as standard I/O....&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[SIZE=2][COLOR=#3f7f5f][SIZE=2][COLOR=#3f7f5f]LPC_IOCON-&amp;gt;PIO0_8 |= 0x02; /* Timer0_16 MAT0 */[/COLOR][/SIZE]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[SIZE=2][COLOR=#3f7f5f]Commented out of init_timer16 in timer16.c[/COLOR][/SIZE]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[/COLOR][/SIZE]&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:38:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Multi-function-pins-on-LPC1343/m-p/580987#M24768</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:38:16Z</dc:date>
    </item>
  </channel>
</rss>