<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Use the uart for nine bits mode with lpc1114 in LPCXpresso IDE</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/Use-the-uart-for-nine-bits-mode-with-lpc1114/m-p/580737#M24657</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Jesse.Rosenberg on Wed Sep 01 15:12:15 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Can you clarify what you mean by 9-bit mode a bit more? I assume you're referring to using a 9th bit for multi device communication (such as with RS-485). If that is the case please take a look at the "rs485" project included with the LPC11xx examples.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 23:58:54 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T23:58:54Z</dc:date>
    <item>
      <title>Use the uart for nine bits mode with lpc1114</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Use-the-uart-for-nine-bits-mode-with-lpc1114/m-p/580736#M24656</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by thinkchip on Wed Sep 01 08:39:37 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;it is possible use the uart of lpc1114 in the mode of 9 bits? in the data sheet I see that only support the 8 bits data, and I don't know if could be possible use the parity bit like the nine bit by software? thanks&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:58:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Use-the-uart-for-nine-bits-mode-with-lpc1114/m-p/580736#M24656</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:58:53Z</dc:date>
    </item>
    <item>
      <title>Re: Use the uart for nine bits mode with lpc1114</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Use-the-uart-for-nine-bits-mode-with-lpc1114/m-p/580737#M24657</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Jesse.Rosenberg on Wed Sep 01 15:12:15 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Can you clarify what you mean by 9-bit mode a bit more? I assume you're referring to using a 9th bit for multi device communication (such as with RS-485). If that is the case please take a look at the "rs485" project included with the LPC11xx examples.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:58:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Use-the-uart-for-nine-bits-mode-with-lpc1114/m-p/580737#M24657</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:58:54Z</dc:date>
    </item>
    <item>
      <title>Re: Use the uart for nine bits mode with lpc1114</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Use-the-uart-for-nine-bits-mode-with-lpc1114/m-p/580738#M24658</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by thinkchip on Wed Sep 01 15:42:45 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Yes, I refer that I could be use the uart with 9 bits data, I try to communicate with a coin changer that use the mdb protocol that use 9 bit data in uart, thanks for the data, best regards&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:58:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Use-the-uart-for-nine-bits-mode-with-lpc1114/m-p/580738#M24658</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:58:54Z</dc:date>
    </item>
    <item>
      <title>Re: Use the uart for nine bits mode with lpc1114</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Use-the-uart-for-nine-bits-mode-with-lpc1114/m-p/580739#M24659</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by thinkchip on Tue Nov 02 20:59:20 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: thinkchip&lt;/STRONG&gt;&lt;BR /&gt;Yes, I refer that I could be use the uart with 9 bits data, I try to communicate with a coin changer that use the mdb protocol that use 9 bit data in uart, thanks for the data, best regards&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi again, I cant configure the uart0 for the LPC1768 for work in 9 bit data mode, is there any example using the uart by software? best regards&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:58:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Use-the-uart-for-nine-bits-mode-with-lpc1114/m-p/580739#M24659</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:58:55Z</dc:date>
    </item>
    <item>
      <title>Re: Use the uart for nine bits mode with lpc1114</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Use-the-uart-for-nine-bits-mode-with-lpc1114/m-p/580740#M24660</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Ex-Zero on Wed Nov 03 04:48:18 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;9-bit Serial Frames are not supported by LPC11xx or LPC17xx UART :( &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;It's possible to use a 9th bit to detect an address in RS485 mode, but that's all.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;AFAIK this 9th bit is used as 'Mode Bit' in MDB, which sounds similar.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: &lt;/STRONG&gt;&lt;BR /&gt;[B][FONT=Arial]Mode Bit: Master-to-Peripheral[/FONT][/B]&lt;BR /&gt;[LEFT][FONT=Arial]The mode bit differentiates between ADDRESS bytes and DATA bytes. ADDRESS[/FONT]&lt;BR /&gt;[FONT=Arial]bytes must be read by all peripherals, DATA bytes are only read by the peripheral that[/FONT]&lt;BR /&gt;[FONT=Arial]has been addressed.[/FONT]&lt;BR /&gt;[FONT=Arial]The mode bit is set (logic one) to indicate an ADDRESS byte, and not set (logic zero) to[/FONT]&lt;BR /&gt;[FONT=Arial]indicate a DATA byte.[/FONT]&lt;BR /&gt;[B][FONT=Arial]Mode Bit: Peripheral-to-Master[/FONT][/B]&lt;BR /&gt;[FONT=Arial]The mode bit must be set on the last byte sent when data is sent from a Slave to the[/FONT][/LEFT]&lt;BR /&gt;[FONT=Arial]Master.[/FONT]&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;So it should be at least possible to read an Address with this 485 sample.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:58:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Use-the-uart-for-nine-bits-mode-with-lpc1114/m-p/580740#M24660</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:58:55Z</dc:date>
    </item>
  </channel>
</rss>