<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LPC1227 half-bridge PWM with deadtime in LPCXpresso IDE</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1227-half-bridge-PWM-with-deadtime/m-p/580704#M24651</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by usafape on Tue Jul 03 07:19:12 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I want a two edge PWM. I will look into MPWM versions. I don't get why anyone would want a single edge PWM. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The control loop has to be fast enough for the bandwidth you need. You can make it work in the right application;)&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jun 2016 02:36:00 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-16T02:36:00Z</dc:date>
    <item>
      <title>LPC1227 half-bridge PWM with deadtime</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1227-half-bridge-PWM-with-deadtime/m-p/580702#M24649</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by usafape on Mon Jul 02 07:40:01 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi all,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Can someone shine me a light if this can be done? If so, can you give me an example? I am trying to drive a synchronous buck converter from it and the PWM outputs are not coming out right. Here's my code:&lt;/SPAN&gt;&lt;BR /&gt;&lt;TABLE border="1"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD bgcolor="#cacaca"&gt; &lt;PRE&gt;
//Setting up the output pins
LPC_IOCON-&amp;gt;PIO2_4 |= 0x03;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // - set bit 1 to connect pin to CT32B0_MAT0
LPC_IOCON-&amp;gt;PIO2_5 |= 0x03;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // - set bit 1 to connect pin to CT32B0_MAT1
&amp;nbsp;&amp;nbsp;&amp;nbsp; LPC_GPIO2-&amp;gt;DIR&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; |= (1 &amp;lt;&amp;lt; 4);&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // - select OUTPUT
&amp;nbsp;&amp;nbsp;&amp;nbsp; LPC_GPIO2-&amp;gt;DIR&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; |= (1 &amp;lt;&amp;lt; 5);&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // - select OUTPUT

&amp;nbsp;&amp;nbsp;&amp;nbsp; LPC_SYSCON-&amp;gt;SYSAHBCLKCTRL |= (1 &amp;lt;&amp;lt; 9); //Enable lock to TMR32B0

&amp;nbsp;&amp;nbsp;&amp;nbsp; LPC_CT32B0-&amp;gt;MCR |= (1 &amp;lt;&amp;lt; 10);

&amp;nbsp;&amp;nbsp;&amp;nbsp; LPC_CT32B0-&amp;gt;MR0 = 1000;
&amp;nbsp;&amp;nbsp;&amp;nbsp; LPC_CT32B0-&amp;gt;MR1 = 1500;
&amp;nbsp;&amp;nbsp;&amp;nbsp; LPC_CT32B0-&amp;gt;MR1 = 2000;
&amp;nbsp;&amp;nbsp;&amp;nbsp; LPC_CT32B0-&amp;gt;MR3 = 2500;

&amp;nbsp;&amp;nbsp;&amp;nbsp; LPC_CT32B0-&amp;gt;PWMC |= (1 &amp;lt;&amp;lt; 0);
&amp;nbsp;&amp;nbsp;&amp;nbsp; LPC_CT32B0-&amp;gt;PWMC |= (1 &amp;lt;&amp;lt; 1);

&amp;nbsp;&amp;nbsp;&amp;nbsp; LPC_CT32B0-&amp;gt;TCR = 1;
&lt;/PRE&gt; &lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks for you help.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 02:35:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1227-half-bridge-PWM-with-deadtime/m-p/580702#M24649</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T02:35:59Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1227 half-bridge PWM with deadtime</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1227-half-bridge-PWM-with-deadtime/m-p/580703#M24650</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Rob65 on Mon Jul 02 13:46:38 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;What is the behaviour that you are looking for?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;"half bridge PWM with dead time" sounds like two PWM outputs with one output being high for a certain time, followed by a 'dead time' (no outputs high) and then the next PWM being high.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;If that is the case, re-read your user manual for the timer operation. As I read it, the timer's PWM outputs are single edge PWMs. If you need double edge PWM signals the you might want to get an LPC1xxx variant that has a MCPWM block for motor control.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;What do you want to do with the buck converter? You do realize that you need a&amp;nbsp; fast control loop to measure and adjust your PWM settings, otherwise your voltage will run away.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I tried to do something like this for high power LEDs but stopped my attempts after the first simulation runs.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Rob&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 02:36:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1227-half-bridge-PWM-with-deadtime/m-p/580703#M24650</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T02:36:00Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1227 half-bridge PWM with deadtime</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1227-half-bridge-PWM-with-deadtime/m-p/580704#M24651</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by usafape on Tue Jul 03 07:19:12 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I want a two edge PWM. I will look into MPWM versions. I don't get why anyone would want a single edge PWM. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The control loop has to be fast enough for the bandwidth you need. You can make it work in the right application;)&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 02:36:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1227-half-bridge-PWM-with-deadtime/m-p/580704#M24651</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T02:36:00Z</dc:date>
    </item>
  </channel>
</rss>