<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDE中的主题 Problem reprogramming flash after WDT enabled</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/Problem-reprogramming-flash-after-WDT-enabled/m-p/580367#M24498</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by jdebliek on Mon Jun 21 10:23:31 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I am working with the LPC11xx, and was testing the release version of the build, which enables the WDT. However, now that the WDT is enabled in the code residing in flash, I cannot reconnect with the debugger (using LPC-link) in order to reprogram the flash. I get the following error:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Error launching Release\&amp;lt;application&amp;gt;.axf&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;03: Failed on chip setup: Et: Flash driver not ready&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Is there any way I can regain access via the debugger now?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 22:38:09 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T22:38:09Z</dc:date>
    <item>
      <title>Problem reprogramming flash after WDT enabled</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Problem-reprogramming-flash-after-WDT-enabled/m-p/580367#M24498</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by jdebliek on Mon Jun 21 10:23:31 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I am working with the LPC11xx, and was testing the release version of the build, which enables the WDT. However, now that the WDT is enabled in the code residing in flash, I cannot reconnect with the debugger (using LPC-link) in order to reprogram the flash. I get the following error:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Error launching Release\&amp;lt;application&amp;gt;.axf&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;03: Failed on chip setup: Et: Flash driver not ready&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Is there any way I can regain access via the debugger now?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:38:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Problem-reprogramming-flash-after-WDT-enabled/m-p/580367#M24498</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:38:09Z</dc:date>
    </item>
    <item>
      <title>Re: Problem reprogramming flash after WDT enabled</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Problem-reprogramming-flash-after-WDT-enabled/m-p/580368#M24499</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by rkiryanov on Mon Jun 21 11:01:47 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Start bootloader - tie ISP pin to GND and reboot MCU.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:38:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Problem-reprogramming-flash-after-WDT-enabled/m-p/580368#M24499</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:38:10Z</dc:date>
    </item>
    <item>
      <title>Re: Problem reprogramming flash after WDT enabled</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Problem-reprogramming-flash-after-WDT-enabled/m-p/580369#M24500</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by yasla on Thu Oct 10 05:22:25 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;You can mass erase before programming too. Works for me.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:38:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Problem-reprogramming-flash-after-WDT-enabled/m-p/580369#M24500</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:38:11Z</dc:date>
    </item>
  </channel>
</rss>