<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDE中的主题 Re: Code Coverage through Gcov</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/Code-Coverage-through-Gcov/m-p/531335#M2443</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is there any update now?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 14 Jan 2017 21:17:15 GMT</pubDate>
    <dc:creator>ls100871</dc:creator>
    <dc:date>2017-01-14T21:17:15Z</dc:date>
    <item>
      <title>Code Coverage through Gcov</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Code-Coverage-through-Gcov/m-p/531333#M2441</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Ramesh on Wed Oct 15 21:51:01 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;is LPC Xpresso will support to Code coverage tool Gcov? if supported what are the precautions need to be taken.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I've tried the steps that are involved in Eclipse as&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;"the user has to compile the C/C++ program with profiling enabled using "-ftest-coverage -fprofile-arcs" options prior to running the tool. These two options must be passed via the project properties to both the compiler (C/C++ Build-&amp;gt;Settings-&amp;gt;Tool Settings-&amp;gt;GCC C Compiler-&amp;gt;Miscellaneous-&amp;gt;Other flags) and the linker (C/C++ Build-&amp;gt;Settings-&amp;gt;Tool Settings-&amp;gt;GCC C Linker-&amp;gt;Miscellaneous-&amp;gt;Linker flags)."&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;but even am unable to get the .gcov file.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;CAn anybody suggest for the same.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Ramesh&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:08:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Code-Coverage-through-Gcov/m-p/531333#M2441</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:08:46Z</dc:date>
    </item>
    <item>
      <title>Re: Code Coverage through Gcov</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Code-Coverage-through-Gcov/m-p/531334#M2442</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by lpcxpresso-support on Thu Oct 16 03:14:06 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Sorry, gcov and gprof is not supported directly by LPCXpresso.&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:08:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Code-Coverage-through-Gcov/m-p/531334#M2442</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:08:47Z</dc:date>
    </item>
    <item>
      <title>Re: Code Coverage through Gcov</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Code-Coverage-through-Gcov/m-p/531335#M2443</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is there any update now?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 14 Jan 2017 21:17:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Code-Coverage-through-Gcov/m-p/531335#M2443</guid>
      <dc:creator>ls100871</dc:creator>
      <dc:date>2017-01-14T21:17:15Z</dc:date>
    </item>
  </channel>
</rss>