<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic stepping problem in LPCXpresso IDE</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/stepping-problem/m-p/580066#M24421</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by mayotte1 on Thu Sep 16 10:11:23 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I have a program that seems to run ok but when I single step in or over some functions,&amp;nbsp; the instructions display are&amp;nbsp; unrelated to the actual functions the program is executing. It eventually works it self back to the next function .Version: LPCXpresso v3.4.6 [Build 199] [11/08/2010] &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Also, sometimes the very first instruction [I]displayed [/I]after a reset is somewhere in the middle of the program. If I step, the actual correct first instruction does execute and then things are back in sync.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Any ideas?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jun 2016 00:03:21 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-16T00:03:21Z</dc:date>
    <item>
      <title>stepping problem</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/stepping-problem/m-p/580066#M24421</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by mayotte1 on Thu Sep 16 10:11:23 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I have a program that seems to run ok but when I single step in or over some functions,&amp;nbsp; the instructions display are&amp;nbsp; unrelated to the actual functions the program is executing. It eventually works it self back to the next function .Version: LPCXpresso v3.4.6 [Build 199] [11/08/2010] &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Also, sometimes the very first instruction [I]displayed [/I]after a reset is somewhere in the middle of the program. If I step, the actual correct first instruction does execute and then things are back in sync.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Any ideas?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:03:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/stepping-problem/m-p/580066#M24421</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T00:03:21Z</dc:date>
    </item>
    <item>
      <title>Re: stepping problem</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/stepping-problem/m-p/580067#M24422</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by CodeRedSupport on Mon Sep 20 02:20:32 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Preferably can you provide a buildable project with instructions on how to replicate? &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;If not, then please provide us with more details so that we can try to replicate. For example:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Is your source code C or assembler?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;What optimisation level are you building for?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Are you stepping at the source level or assembler level?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Are your "problem" functions in you main project or in library projects?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Can you provide screenshots showing the problem as you progress through your application?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;CodeRedSupport&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:03:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/stepping-problem/m-p/580067#M24422</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T00:03:22Z</dc:date>
    </item>
  </channel>
</rss>