<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: On-chip rom driver + ReInvokeISP in LPC1343 in LPCXpresso IDE</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/On-chip-rom-driver-ReInvokeISP-in-LPC1343/m-p/579940#M24318</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by kendwyer on Mon Apr 11 17:22:09 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;There is an example for CDC/MSC Composite device here:&lt;/SPAN&gt;&lt;BR /&gt;&lt;A href="http://"&gt;http://ics.nxp.com/support/documents/microcontrollers/zip/an11018.zip&lt;/A&gt;&lt;BR /&gt;&lt;SPAN&gt;Not sure if it is possible to do this with the USB BootROM code.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 22:41:11 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T22:41:11Z</dc:date>
    <item>
      <title>On-chip rom driver + ReInvokeISP in LPC1343</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/On-chip-rom-driver-ReInvokeISP-in-LPC1343/m-p/579937#M24315</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by jush on Mon Apr 11 00:28:36 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;[FONT=Arial][SIZE=2]I have an application code for firmware development which is run on LPC1343, the source code contains the&amp;nbsp; codes of usbhidrom(one function for this) and autoisp which is calling the ISP bootloader(one function).&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I simply call the the function of HIDrom and ReInvokeISP in the main function. During debugging only the ISPBootloader is enumerated or found in the device manager, while the HIDRom is not. If I comment out the function of ispbootloader and run the application, the HIDrom is working. So what's the reason why this thing happened? Could someone explain me about this? Why is it if the two function is running, only the ispbootloader is executed?what happen for the usb hid?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;:confused::confused::confused::confused:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks.[/SIZE][/FONT]&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:41:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/On-chip-rom-driver-ReInvokeISP-in-LPC1343/m-p/579937#M24315</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:41:09Z</dc:date>
    </item>
    <item>
      <title>Re: On-chip rom driver + ReInvokeISP in LPC1343</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/On-chip-rom-driver-ReInvokeISP-in-LPC1343/m-p/579938#M24316</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by TheFallGuy on Mon Apr 11 01:21:12 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I think that to enumerate as multiple devices, you need to be a USB Composite device.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:41:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/On-chip-rom-driver-ReInvokeISP-in-LPC1343/m-p/579938#M24316</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:41:10Z</dc:date>
    </item>
    <item>
      <title>Re: On-chip rom driver + ReInvokeISP in LPC1343</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/On-chip-rom-driver-ReInvokeISP-in-LPC1343/m-p/579939#M24317</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by jush on Mon Apr 11 01:44:08 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;So it is possible to create a composite device for usbhid on-chip rom together with bootloader?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;How, coud I do that?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:41:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/On-chip-rom-driver-ReInvokeISP-in-LPC1343/m-p/579939#M24317</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:41:11Z</dc:date>
    </item>
    <item>
      <title>Re: On-chip rom driver + ReInvokeISP in LPC1343</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/On-chip-rom-driver-ReInvokeISP-in-LPC1343/m-p/579940#M24318</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by kendwyer on Mon Apr 11 17:22:09 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;There is an example for CDC/MSC Composite device here:&lt;/SPAN&gt;&lt;BR /&gt;&lt;A href="http://"&gt;http://ics.nxp.com/support/documents/microcontrollers/zip/an11018.zip&lt;/A&gt;&lt;BR /&gt;&lt;SPAN&gt;Not sure if it is possible to do this with the USB BootROM code.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:41:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/On-chip-rom-driver-ReInvokeISP-in-LPC1343/m-p/579940#M24318</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:41:11Z</dc:date>
    </item>
  </channel>
</rss>