<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDE中的主题 LPC1347 PIO0_12/TMS no Input</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1347-PIO0-12-TMS-no-Input/m-p/531261#M2415</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Michael65589 on Wed Jun 26 02:19:46 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I want to use the PIO0_12 as capture input.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I turn on the clock for IOCON and CT32B1. Set the func of PIO0_12 to 0x3 (CT32B1_CAP0). I also activate the interrupts for CT32B1_CAP0 CCR-&amp;gt; 0x6 but there is no interrupt.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I use the same code on an LPC1313 with PIO1_0 as input pin and there the code is running.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;It seems that the signal on PIO0_12 does not activate an interrupt. Is there something special with PIO0_12 because the default value is TMS?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Best regards&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Michael&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jun 2016 01:35:59 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-16T01:35:59Z</dc:date>
    <item>
      <title>LPC1347 PIO0_12/TMS no Input</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1347-PIO0-12-TMS-no-Input/m-p/531261#M2415</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Michael65589 on Wed Jun 26 02:19:46 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I want to use the PIO0_12 as capture input.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I turn on the clock for IOCON and CT32B1. Set the func of PIO0_12 to 0x3 (CT32B1_CAP0). I also activate the interrupts for CT32B1_CAP0 CCR-&amp;gt; 0x6 but there is no interrupt.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I use the same code on an LPC1313 with PIO1_0 as input pin and there the code is running.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;It seems that the signal on PIO0_12 does not activate an interrupt. Is there something special with PIO0_12 because the default value is TMS?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Best regards&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Michael&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 01:35:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1347-PIO0-12-TMS-no-Input/m-p/531261#M2415</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T01:35:59Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1347 PIO0_12/TMS no Input</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1347-PIO0-12-TMS-no-Input/m-p/531262#M2416</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Michael65589 on Wed Jun 26 03:47:24 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I found the reason by myself. I wrote to the IOCON register 0x3 for the PIO0_12 to set the function to CT32B1_CAP0 but by writing 0x3 I also set the ADMODE of this pin to analog input mode. I had to or the register with 0x3 then it works well.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 01:36:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1347-PIO0-12-TMS-no-Input/m-p/531262#M2416</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T01:36:00Z</dc:date>
    </item>
  </channel>
</rss>