<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Relative path for linked resource? in LPCXpresso IDE</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/Relative-path-for-linked-resource/m-p/579431#M24108</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by jdebliek on Mon Jun 21 12:11:26 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I am sharing some code between two projects in the same workspace.&amp;nbsp; I do not want to generate a library, but want to compile the code within each project.&amp;nbsp; The only way I found to do this without duplicating the code was to create a linked resource path variable pointing to the shared code.&amp;nbsp; However, this path variable is an absolute path, which means the workspace is no longer completely portable.&amp;nbsp; Is there any way to create a linked resource using a relative path?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 22:38:08 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T22:38:08Z</dc:date>
    <item>
      <title>Relative path for linked resource?</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Relative-path-for-linked-resource/m-p/579431#M24108</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by jdebliek on Mon Jun 21 12:11:26 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I am sharing some code between two projects in the same workspace.&amp;nbsp; I do not want to generate a library, but want to compile the code within each project.&amp;nbsp; The only way I found to do this without duplicating the code was to create a linked resource path variable pointing to the shared code.&amp;nbsp; However, this path variable is an absolute path, which means the workspace is no longer completely portable.&amp;nbsp; Is there any way to create a linked resource using a relative path?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:38:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Relative-path-for-linked-resource/m-p/579431#M24108</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:38:08Z</dc:date>
    </item>
    <item>
      <title>Re: Relative path for linked resource?</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Relative-path-for-linked-resource/m-p/579432#M24109</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by CodeRedSupport on Tue Jun 22 00:47:13 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Relative paths are not supported for linked resources. However, you can use a Path Variable so that you only need to change a path location in one place.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Search the help for "Path Variable" for details.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:38:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Relative-path-for-linked-resource/m-p/579432#M24109</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:38:09Z</dc:date>
    </item>
  </channel>
</rss>