<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDE中的主题 SPI Interrupt</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/SPI-Interrupt/m-p/579197#M24000</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Philipp on Fri Nov 12 04:24:50 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I have a problem with the SPI Interrupt. I enabled the RTIM Interrupt. I get this interrupt after the second data frame and after a periode of 125us. The Time depends on the Frequency. Is there an other solution of getting an Interrupt without asking the RNE status Bit permanently?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;And is it correct that the Interrupt triggers after the second Data? Is there an Option to set this variable.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks for Help&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jun 2016 01:11:40 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-16T01:11:40Z</dc:date>
    <item>
      <title>SPI Interrupt</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/SPI-Interrupt/m-p/579197#M24000</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Philipp on Fri Nov 12 04:24:50 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I have a problem with the SPI Interrupt. I enabled the RTIM Interrupt. I get this interrupt after the second data frame and after a periode of 125us. The Time depends on the Frequency. Is there an other solution of getting an Interrupt without asking the RNE status Bit permanently?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;And is it correct that the Interrupt triggers after the second Data? Is there an Option to set this variable.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks for Help&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 01:11:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/SPI-Interrupt/m-p/579197#M24000</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T01:11:40Z</dc:date>
    </item>
    <item>
      <title>Re: SPI Interrupt</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/SPI-Interrupt/m-p/579198#M24001</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Philipp on Mon Nov 15 04:12:00 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Okay I found the Problem. The Time between Command 1 and 2 was too short. The second fault, the Time till the Interrupt was too high because my Registers were badly set. My SPICLOCKDIV was 2, I set it now on 1. That's a faktor of 2.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;To reduce the time, I set the CLOCK PRESCALE REGISTER on a higher number. With CPR of 6 now, I have an Interrupt Time of&amp;nbsp; 5us.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Can anyone explain me, how this number compose? Is there a Formula?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks for help&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 01:11:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/SPI-Interrupt/m-p/579198#M24001</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T01:11:41Z</dc:date>
    </item>
  </channel>
</rss>