<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDE中的主题 LPCXpresso and LPC-Link without source code</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPCXpresso-and-LPC-Link-without-source-code/m-p/579117#M23970</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by ldd on Fri May 31 09:58:15 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Is it possible to use LPCXpresso with LPC-Link to program a .axf or .bin file into my processor and then receive messages back via the console window without all of the source code in a project.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The reason: Production need to program devices and receive the results of self test and I don't want them to be able to corrupt the code.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Or maybe there is a better way. Any ideas welcome.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jun 2016 02:33:32 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-16T02:33:32Z</dc:date>
    <item>
      <title>LPCXpresso and LPC-Link without source code</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPCXpresso-and-LPC-Link-without-source-code/m-p/579117#M23970</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by ldd on Fri May 31 09:58:15 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Is it possible to use LPCXpresso with LPC-Link to program a .axf or .bin file into my processor and then receive messages back via the console window without all of the source code in a project.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The reason: Production need to program devices and receive the results of self test and I don't want them to be able to corrupt the code.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Or maybe there is a better way. Any ideas welcome.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 02:33:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPCXpresso-and-LPC-Link-without-source-code/m-p/579117#M23970</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T02:33:32Z</dc:date>
    </item>
    <item>
      <title>Re: LPCXpresso and LPC-Link without source code</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPCXpresso-and-LPC-Link-without-source-code/m-p/579118#M23971</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by R2D2 on Fri May 31 10:36:57 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: ldd&lt;/STRONG&gt;&lt;BR /&gt;Or maybe there is a better way. Any ideas welcome.&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm using 'GUI flash programming tool' with test program as AXF and UART output. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;A href="http://"&gt;http://www.support.code-red-tech.com/CodeRedWiki/GuiFlashProgramming&lt;/A&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 02:33:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPCXpresso-and-LPC-Link-without-source-code/m-p/579118#M23971</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T02:33:33Z</dc:date>
    </item>
    <item>
      <title>Re: LPCXpresso and LPC-Link without source code</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPCXpresso-and-LPC-Link-without-source-code/m-p/579119#M23972</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by ldd on Mon Jun 03 02:57:28 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;The UART is already in use within the board so I have to use the debug port for self-test reporting as it is the only wired connection available to the outside world.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I have found that I can use any project, copy my .axf file into it and set up a debug configuration that doesn't perform a rebuild and points to my .axf file.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The debugger then may tell me that it cannot find the source code but it still programs and runs my .axf file.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 02:33:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPCXpresso-and-LPC-Link-without-source-code/m-p/579119#M23972</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T02:33:34Z</dc:date>
    </item>
  </channel>
</rss>