<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDEのトピックRe: Possible to debug LPC1343 LPCXpresso board while using USB port?</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/Possible-to-debug-LPC1343-LPCXpresso-board-while-using-USB-port/m-p/578369#M23626</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Thilo on Tue May 31 15:23:13 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;thanks. The user manual you linked provides an example for using the usb connector, but it also mentions that it's not the "right way" to do it. Where can I find information for a complete connection circuit?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thilo&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 23:58:31 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T23:58:31Z</dc:date>
    <item>
      <title>Possible to debug LPC1343 LPCXpresso board while using USB port?</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Possible-to-debug-LPC1343-LPCXpresso-board-while-using-USB-port/m-p/578367#M23624</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Thilo on Tue May 31 13:56:56 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm considering to get myself a LPC1343 LPCXpresso board to prototype a HID device, but I am wondering if it is possible to use the debugger on a program that uses the USB port to register the device as an HID. So, is it possible?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thilo&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:58:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Possible-to-debug-LPC1343-LPCXpresso-board-while-using-USB-port/m-p/578367#M23624</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:58:29Z</dc:date>
    </item>
    <item>
      <title>Re: Possible to debug LPC1343 LPCXpresso board while using USB port?</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Possible-to-debug-LPC1343-LPCXpresso-board-while-using-USB-port/m-p/578368#M23625</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Ex-Zero on Tue May 31 14:19:56 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;That's not the same USB port. LPCXpresso's USB is used for LC-Link (=Debugger via SWD).&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;You have to add another USB connector to use the target board USB, so debugging target USB is possible :)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;See #9 of:&lt;/SPAN&gt;&lt;BR /&gt;&lt;A href="http://"&gt;http://knowledgebase.nxp.trimm.net/showthread.php?t=505&lt;/A&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Also:&lt;/SPAN&gt;&lt;BR /&gt;&lt;A href="http://"&gt;http://ics.nxp.com/support/documents/microcontrollers/pdf/lpcxpresso.getting.started.pdf&lt;/A&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:58:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Possible-to-debug-LPC1343-LPCXpresso-board-while-using-USB-port/m-p/578368#M23625</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:58:30Z</dc:date>
    </item>
    <item>
      <title>Re: Possible to debug LPC1343 LPCXpresso board while using USB port?</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Possible-to-debug-LPC1343-LPCXpresso-board-while-using-USB-port/m-p/578369#M23626</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Thilo on Tue May 31 15:23:13 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;thanks. The user manual you linked provides an example for using the usb connector, but it also mentions that it's not the "right way" to do it. Where can I find information for a complete connection circuit?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thilo&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:58:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Possible-to-debug-LPC1343-LPCXpresso-board-while-using-USB-port/m-p/578369#M23626</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:58:31Z</dc:date>
    </item>
    <item>
      <title>Re: Possible to debug LPC1343 LPCXpresso board while using USB port?</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Possible-to-debug-LPC1343-LPCXpresso-board-while-using-USB-port/m-p/578370#M23627</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Ex-Zero on Tue May 31 15:41:10 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;The right way is to use a transistor (or more elegant a FET) as shown in my schematic / board to switch 1.5k pullup to D+ :)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;So USB_VBUS and USB_CONNECT can be used.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Schematic:&lt;/SPAN&gt;&lt;BR /&gt;&lt;A href="http://http://www.flickr.com/photos/58892165@N08/5406160762/"&gt;[COLOR=#5174a3]http://www.flickr.com/photos/58892165@N08/5406160762/[/COLOR]&lt;/A&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Board:&lt;/SPAN&gt;&lt;BR /&gt;&lt;A href="http://http://www.flickr.com/photos/58892165@N08/5406160872/"&gt;[COLOR=#5174a3]http://www.flickr.com/photos/58892165@N08/5406160872/[/COLOR]&lt;/A&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:58:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Possible-to-debug-LPC1343-LPCXpresso-board-while-using-USB-port/m-p/578370#M23627</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:58:32Z</dc:date>
    </item>
    <item>
      <title>Re: Possible to debug LPC1343 LPCXpresso board while using USB port?</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Possible-to-debug-LPC1343-LPCXpresso-board-while-using-USB-port/m-p/578371#M23628</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Lumen on Tue Apr 03 06:51:23 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: Zero&lt;/STRONG&gt;&lt;BR /&gt;The right way is to use a transistor (or more elegant a FET) as shown in my schematic / board to switch 1.5k pullup to D+ :)&lt;BR /&gt; &lt;BR /&gt;So USB_VBUS and USB_CONNECT can be used.&lt;BR /&gt; &lt;BR /&gt;Schematic:&lt;BR /&gt;&lt;A href="http://http://www.flickr.com/photos/58892165@N08/5406160762/"&gt;[COLOR=#5174a3]http://www.flickr.com/photos/58892165@N08/5406160762/[/COLOR]&lt;/A&gt;&lt;BR /&gt; &lt;BR /&gt; &lt;BR /&gt;Board:&lt;BR /&gt;&lt;A href="http://http://www.flickr.com/photos/58892165@N08/5406160872/"&gt;[COLOR=#5174a3]http://www.flickr.com/photos/58892165@N08/5406160872/[/COLOR]&lt;/A&gt;&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thank you Zero, thats the FET I was looking for :-)&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:58:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Possible-to-debug-LPC1343-LPCXpresso-board-while-using-USB-port/m-p/578371#M23628</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:58:32Z</dc:date>
    </item>
  </channel>
</rss>