<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDE中的主题 Re: Interrupt level sensitivity</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/Interrupt-level-sensitivity/m-p/578351#M23618</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by igorsk on Wed Apr 14 17:52:02 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;With level sensitive, you'll keep getting interrupts as long as the input remains active (low or high). With edge-sensitive it will happen only once per level transition.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jun 2016 02:30:57 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-16T02:30:57Z</dc:date>
    <item>
      <title>Interrupt level sensitivity</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Interrupt-level-sensitivity/m-p/578350#M23617</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by LynnF on Wed Apr 14 17:25:28 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Can someone please offer an explanation of the following, please.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Edge sensitive is obvious but what is "level sensitive"? I would assume a steady state has been reached, and if correct how long is the steady state before the interrupt is generated?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[FONT=Arial][SIZE=1]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[LEFT][/SIZE][/FONT][B][FONT=Arial][SIZE=1][COLOR=#005042][FONT=Arial][SIZE=1][COLOR=#005042][FONT=Arial][SIZE=1][COLOR=#005042]Table 111. GPIOnIS register (GPIO0IS, address 0x5000 8004 to GPIO3IS, address 0x5003[/COLOR][/SIZE][/FONT][/COLOR][/SIZE][/FONT][/COLOR][/SIZE][/FONT][/B][FONT=Arial][SIZE=1][COLOR=#005042][FONT=Arial][SIZE=1][COLOR=#005042]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[B][SIZE=1][FONT=Arial][COLOR=#005042]8004) bit description[/COLOR][/FONT][/SIZE][/B]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[/COLOR][/SIZE][/FONT][/COLOR][/SIZE][/FONT][B][FONT=Arial][SIZE=1][FONT=Arial][SIZE=1]Bit Symbol Access Value Description Reset[/SIZE][/FONT][/SIZE][/FONT][/B][FONT=Arial][SIZE=1]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[B][SIZE=1][FONT=Arial]value[/FONT][/SIZE][/B]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[/SIZE][/FONT][FONT=Arial][SIZE=1][FONT=Arial][SIZE=1]11:0 ISENSE R/W Selects interrupt on pin x as level or edge sensitive[/SIZE][/FONT]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[SIZE=1][FONT=Arial](x = 0 to 11).[/FONT][/SIZE]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[SIZE=1][FONT=Arial]0x00[/FONT][/SIZE]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[SIZE=1][FONT=Arial]0 Interrupt on pin PIOn_x is configured as edge[/FONT][/SIZE]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[SIZE=1][FONT=Arial]sensitive.[/FONT][/SIZE]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[SIZE=1][FONT=Arial]1 Interrupt on pin PIOn_x is configured as [COLOR=red]level[/COLOR][/FONT][/SIZE]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[SIZE=1][FONT=Arial][COLOR=red]sensitive.[/COLOR][/FONT][/SIZE][/LEFT]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[/SIZE][/FONT]&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 02:30:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Interrupt-level-sensitivity/m-p/578350#M23617</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T02:30:56Z</dc:date>
    </item>
    <item>
      <title>Re: Interrupt level sensitivity</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Interrupt-level-sensitivity/m-p/578351#M23618</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by igorsk on Wed Apr 14 17:52:02 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;With level sensitive, you'll keep getting interrupts as long as the input remains active (low or high). With edge-sensitive it will happen only once per level transition.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 02:30:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Interrupt-level-sensitivity/m-p/578351#M23618</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T02:30:57Z</dc:date>
    </item>
  </channel>
</rss>