<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDE中的主题 Re: Differences LPC2362 and LPC2368</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/Differences-LPC2362-and-LPC2368/m-p/578137#M23500</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by rkiryanov on Thu Jun 17 00:18:22 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Remark: On reset, UART0 is enabled (PCUART0 = 1), and UART2/3 are disabled&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;(PCUART2/3 = 0).&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 22:39:32 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T22:39:32Z</dc:date>
    <item>
      <title>Differences LPC2362 and LPC2368</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Differences-LPC2362-and-LPC2368/m-p/578136#M23499</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by finfo on Thu Jun 17 00:14:34 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I am working on a prototype with the LPC2362.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I would say the hardware is working.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Now I am trying to implement a software originally written with the Keil IDE.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I got the original hex file. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;In the original device is the UART0 used to receive data. Then the software is switched to the UART3 for my device. (has another reason not important here)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;This is included in the hex file.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;When I am using flashmagic to write that software into the device it is not working on the UART3 side. I could tell that because in the debug mode the same occurs.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Now is my question is there anything different on the LPC2362 to the LPC2368 device which could be the reason for that? The flash size is not the problem because I don't fill the128kB.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thank for any ideas!&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Florian&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:39:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Differences-LPC2362-and-LPC2368/m-p/578136#M23499</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:39:31Z</dc:date>
    </item>
    <item>
      <title>Re: Differences LPC2362 and LPC2368</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Differences-LPC2362-and-LPC2368/m-p/578137#M23500</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by rkiryanov on Thu Jun 17 00:18:22 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Remark: On reset, UART0 is enabled (PCUART0 = 1), and UART2/3 are disabled&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;(PCUART2/3 = 0).&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:39:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Differences-LPC2362-and-LPC2368/m-p/578137#M23500</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:39:32Z</dc:date>
    </item>
    <item>
      <title>Re: Differences LPC2362 and LPC2368</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Differences-LPC2362-and-LPC2368/m-p/578138#M23501</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by finfo on Thu Jun 17 03:27:41 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;If I reset the device it runs my init function which includes to set the enable bit.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;anymore suggestions?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Florian&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:39:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Differences-LPC2362-and-LPC2368/m-p/578138#M23501</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:39:32Z</dc:date>
    </item>
    <item>
      <title>Re: Differences LPC2362 and LPC2368</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Differences-LPC2362-and-LPC2368/m-p/578139#M23502</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by kendwyer on Thu Jun 17 20:04:58 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Flashmagic and ISP work hand in hand and would need to use the UART0.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I am not sure why you are mentioning the LPC2368 in you description but that device would behave the same way.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Ken&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:39:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Differences-LPC2362-and-LPC2368/m-p/578139#M23502</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:39:33Z</dc:date>
    </item>
  </channel>
</rss>