<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDE中的主题 Re: Get rid of LPCXpresso built-in include paths</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/Get-rid-of-LPCXpresso-built-in-include-paths/m-p/577704#M23320</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by pkold on Tue May 01 05:51:42 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Never mind - found it myself&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;So this is what "Properties-&amp;gt;C/C++ Build-&amp;gt;Discovery Options" are used for&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jun 2016 01:08:49 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-16T01:08:49Z</dc:date>
    <item>
      <title>Get rid of LPCXpresso built-in include paths</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Get-rid-of-LPCXpresso-built-in-include-paths/m-p/577703#M23319</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by pkold on Tue May 01 05:11:29 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;How do I get rid of the built-in include paths?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;In Project-&amp;gt;Properties-&amp;gt;C/C++ General-&amp;gt;Paths and Symbols under "Additional Assembly Source Files" and "GNU C" 3 include folders are always present and the "Delete" button is grayed so they can't be deleted from here.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The folders are named something like:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;..arm-none-eabi/4.5.1/include&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;..arm-none-eabi/4.5.1/include-fixed&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;..arm-none-eabi/include&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I prefer to manually control which folders are searched.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 01:08:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Get-rid-of-LPCXpresso-built-in-include-paths/m-p/577703#M23319</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T01:08:48Z</dc:date>
    </item>
    <item>
      <title>Re: Get rid of LPCXpresso built-in include paths</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Get-rid-of-LPCXpresso-built-in-include-paths/m-p/577704#M23320</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by pkold on Tue May 01 05:51:42 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Never mind - found it myself&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;So this is what "Properties-&amp;gt;C/C++ Build-&amp;gt;Discovery Options" are used for&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 01:08:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Get-rid-of-LPCXpresso-built-in-include-paths/m-p/577704#M23320</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T01:08:49Z</dc:date>
    </item>
  </channel>
</rss>