<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDEのトピックLPCXpresso and MinGW</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPCXpresso-and-MinGW/m-p/577688#M23317</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by piperazine on Thu Mar 31 16:20:06 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I've just had to install MinGW along with Eclipse just to do some testing of C/C++ programs/functions, and it got me thinking to weather I could use LPCXpresso IDE instead of the standard Eclipse one. So I had a little play and managed to create a C project using the MinGW toolchain in LPCXpresso using the project wizard. I got it to build and run (by right clicking project-&amp;gt;Run as-&amp;gt;local C/C++ application).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I thought I might try and push my luck to see if I could debug it (I right clicked project-&amp;gt;Debug as-&amp;gt;local C/C++ application) but no joy (error window pops up).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Is it posible to get debug to work with MinGW projects in LPCXpresso, or is this not possible(I would say supported, but I kinda know the answer to that :D).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;....just curious&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 22:34:44 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T22:34:44Z</dc:date>
    <item>
      <title>LPCXpresso and MinGW</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPCXpresso-and-MinGW/m-p/577688#M23317</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by piperazine on Thu Mar 31 16:20:06 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I've just had to install MinGW along with Eclipse just to do some testing of C/C++ programs/functions, and it got me thinking to weather I could use LPCXpresso IDE instead of the standard Eclipse one. So I had a little play and managed to create a C project using the MinGW toolchain in LPCXpresso using the project wizard. I got it to build and run (by right clicking project-&amp;gt;Run as-&amp;gt;local C/C++ application).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I thought I might try and push my luck to see if I could debug it (I right clicked project-&amp;gt;Debug as-&amp;gt;local C/C++ application) but no joy (error window pops up).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Is it posible to get debug to work with MinGW projects in LPCXpresso, or is this not possible(I would say supported, but I kinda know the answer to that :D).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;....just curious&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:34:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPCXpresso-and-MinGW/m-p/577688#M23317</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:34:44Z</dc:date>
    </item>
  </channel>
</rss>