<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDEのトピックLPC1769 USB device not recognized</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1769-USB-device-not-recognized/m-p/530989#M2266</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by yan6 on Thu Dec 26 14:47:33 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi there, I'm having troubles getting the LPC-Link to connect via usb. I have tried it on Windows 7 &amp;amp; on XP, both with the same results. On both OS' I have tried manually to install the drivers by pointing the unknown device to the driver directory; I have tried installing the *.inf file and have tried to manually register the *.Dll's that are located in the driver directory, but receive an error.&amp;nbsp; &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;On the LPC board I am receiving 2 blinks on the LED while plugged into the computer&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Can anyone offer some further suggestions &lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jun 2016 02:54:33 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-16T02:54:33Z</dc:date>
    <item>
      <title>LPC1769 USB device not recognized</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1769-USB-device-not-recognized/m-p/530989#M2266</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by yan6 on Thu Dec 26 14:47:33 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi there, I'm having troubles getting the LPC-Link to connect via usb. I have tried it on Windows 7 &amp;amp; on XP, both with the same results. On both OS' I have tried manually to install the drivers by pointing the unknown device to the driver directory; I have tried installing the *.inf file and have tried to manually register the *.Dll's that are located in the driver directory, but receive an error.&amp;nbsp; &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;On the LPC board I am receiving 2 blinks on the LED while plugged into the computer&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Can anyone offer some further suggestions &lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 02:54:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1769-USB-device-not-recognized/m-p/530989#M2266</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T02:54:33Z</dc:date>
    </item>
  </channel>
</rss>