<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDE中的主题 Re: Debug does not succeed unless I start RedlinkServ manually. (RedProbe +)</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/Debug-does-not-succeed-unless-I-start-RedlinkServ-manually/m-p/575431#M22298</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The window&amp;nbsp;pops back up, empty as in the first image above. Once I run redlinkserv from the command prompt I can click search for linkserveragain and it will work.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I click search for emulator, it behaves the same way. No options until I launch redlinkserv manually.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is still a very big problem. Thanks in advance for your help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 14 Sep 2016 20:10:54 GMT</pubDate>
    <dc:creator>mj7man</dc:creator>
    <dc:date>2016-09-14T20:10:54Z</dc:date>
    <item>
      <title>Debug does not succeed unless I start RedlinkServ manually. (RedProbe +)</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Debug-does-not-succeed-unless-I-start-RedlinkServ-manually/m-p/575429#M22296</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Community, I'm new here, however I have been searching online for solutions and have attempted several things and nothing has worked yet.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Symptoms:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;When I launch debug LPCXpresso does not find "an emulator" (debugger). The first time or two I launched it a Windows firewall dialog came up, I have allowed it and verified that the entry is in the firewall. (it appears on the inbound side).&lt;/LI&gt;&lt;LI&gt;If I launch the redlinkserv.exe executable from the command line, then attempt debug from lpcxpresso, my probe is found and everything works as expected.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;It appears to me that lpcxpresso is somehow failing to start the server. The issue with my workaround is that once I stop the debug it kills the redlinkserv process and I have to relaunch it each time I run debug. I don't want to have to do that.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm running&amp;nbsp;LPCXpresso v8.2.0 [Build 647] [2016-07-18]&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="error.PNG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/2751iB6A70066A1D1540F/image-size/large?v=v2&amp;amp;px=999" role="button" title="error.PNG" alt="error.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="force it to work.PNG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/2808iE6414C82623D154A/image-size/large?v=v2&amp;amp;px=999" role="button" title="force it to work.PNG" alt="force it to work.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 Aug 2016 23:07:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Debug-does-not-succeed-unless-I-start-RedlinkServ-manually/m-p/575429#M22296</guid>
      <dc:creator>mj7man</dc:creator>
      <dc:date>2016-08-30T23:07:34Z</dc:date>
    </item>
    <item>
      <title>Re: Debug does not succeed unless I start RedlinkServ manually. (RedProbe +)</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Debug-does-not-succeed-unless-I-start-RedlinkServ-manually/m-p/575430#M22297</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;With your Red Probe+ connected, what happens when you press the "Search for any enabled emulator" button?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and regards,&lt;/P&gt;&lt;P&gt;LPCXpresso Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Sep 2016 20:48:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Debug-does-not-succeed-unless-I-start-RedlinkServ-manually/m-p/575430#M22297</guid>
      <dc:creator>lpcxpresso_supp</dc:creator>
      <dc:date>2016-09-12T20:48:08Z</dc:date>
    </item>
    <item>
      <title>Re: Debug does not succeed unless I start RedlinkServ manually. (RedProbe +)</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Debug-does-not-succeed-unless-I-start-RedlinkServ-manually/m-p/575431#M22298</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The window&amp;nbsp;pops back up, empty as in the first image above. Once I run redlinkserv from the command prompt I can click search for linkserveragain and it will work.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I click search for emulator, it behaves the same way. No options until I launch redlinkserv manually.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is still a very big problem. Thanks in advance for your help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Sep 2016 20:10:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Debug-does-not-succeed-unless-I-start-RedlinkServ-manually/m-p/575431#M22298</guid>
      <dc:creator>mj7man</dc:creator>
      <dc:date>2016-09-14T20:10:54Z</dc:date>
    </item>
    <item>
      <title>Re: Debug does not succeed unless I start RedlinkServ manually. (RedProbe +)</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Debug-does-not-succeed-unless-I-start-RedlinkServ-manually/m-p/575432#M22299</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm sorry to hear that you are still having problems.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you please try switching to a completely new workspace, create a new "Hello world" project for your target MCU using the new project wizard, then try debugging that. Can you then successfully start a debug session, or do you&amp;nbsp;still need to start Redlinkserver&amp;nbsp;manually?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Something else to try would be to remove any non-essential USB devices from your system. And if you are using a dock of some description, try starting a debug session when not docked.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you are still having problems, can you please confirm the exact version of Windows&amp;nbsp;that you are using (and also whether this is &amp;nbsp;an English or another local?&amp;nbsp;Can you also ZIP up and post the .metadata\.log file from within your new workspace directory.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;LPCXpresso Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Sep 2016 12:55:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Debug-does-not-succeed-unless-I-start-RedlinkServ-manually/m-p/575432#M22299</guid>
      <dc:creator>lpcxpresso_supp</dc:creator>
      <dc:date>2016-09-15T12:55:42Z</dc:date>
    </item>
  </channel>
</rss>