<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LPC13xx Composite Device in LPCXpresso IDE</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC13xx-Composite-Device/m-p/574621#M21933</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by jush on Fri Apr 01 01:48:49 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I run the example about creating a composite device of USB, it is about MSC and CDC combination.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I want to create a composite device using HID ROM and MSC ROM.It is possible to combine this two (using on-chip ROM)?I already do like as describe in&amp;nbsp; the document but still when i run the project it didn't enumerate the MSC and HID.:confused:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Someone could help me about this?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 22:34:33 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T22:34:33Z</dc:date>
    <item>
      <title>LPC13xx Composite Device</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC13xx-Composite-Device/m-p/574621#M21933</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by jush on Fri Apr 01 01:48:49 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I run the example about creating a composite device of USB, it is about MSC and CDC combination.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I want to create a composite device using HID ROM and MSC ROM.It is possible to combine this two (using on-chip ROM)?I already do like as describe in&amp;nbsp; the document but still when i run the project it didn't enumerate the MSC and HID.:confused:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Someone could help me about this?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:34:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC13xx-Composite-Device/m-p/574621#M21933</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:34:33Z</dc:date>
    </item>
  </channel>
</rss>