<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Wakeup as ADC trigger in LPCXpresso IDE</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/Wakeup-as-ADC-trigger/m-p/574521#M21895</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by ruchika123 on Mon Feb 22 21:51:54 MST 2016&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I am using the LPCXpresso board with LPC1549. I have got a wakeup switch on the board which i want to use as the hardware trigger for the ADC but when i assign PINTRIG0 or PINTRIG1 to the pin connected to the wakeup button on the board which is PO0_17, i cannot use it as a trigger. For testing that pin as the trigger i toggle the onboard LED to test its triggering but the LED does not toggle. I cannot get any detailed information wheather PO0_17 can be used as an external trigger or not. I need help on this.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Ruchika&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 22:33:11 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T22:33:11Z</dc:date>
    <item>
      <title>Wakeup as ADC trigger</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Wakeup-as-ADC-trigger/m-p/574521#M21895</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by ruchika123 on Mon Feb 22 21:51:54 MST 2016&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I am using the LPCXpresso board with LPC1549. I have got a wakeup switch on the board which i want to use as the hardware trigger for the ADC but when i assign PINTRIG0 or PINTRIG1 to the pin connected to the wakeup button on the board which is PO0_17, i cannot use it as a trigger. For testing that pin as the trigger i toggle the onboard LED to test its triggering but the LED does not toggle. I cannot get any detailed information wheather PO0_17 can be used as an external trigger or not. I need help on this.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Ruchika&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:33:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Wakeup-as-ADC-trigger/m-p/574521#M21895</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:33:11Z</dc:date>
    </item>
  </channel>
</rss>