<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDE中的主题 Re: Issues while program flash multiple device</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/Issues-while-program-flash-multiple-device/m-p/573809#M21610</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by partheepan on Thu Sep 10 05:01:49 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks for your reply.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Could you please let me know where could I find the parameters and could you please give me an example command line as it would be a great help.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 23:52:42 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T23:52:42Z</dc:date>
    <item>
      <title>Issues while program flash multiple device</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Issues-while-program-flash-multiple-device/m-p/573807#M21608</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by partheepan on Wed Sep 09 06:31:21 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I am using a couple of lpc824 boards (OM13071).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have connected them to a single pc and trying to flash program them by selecting the device from the connect to emulator pop up. Whichever device I select the same device is programmed again and again and not the other one by the GUI.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I tried coping the flash command from GUI and got this one &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;crt_emu_cm_redlink -flash-load-exec "C:\Users\elpk5\Documents\LPCXpresso_7.8.0_426\workspace\i2cTest\Debug\i2cTest.axf" -g -2&amp;nbsp; -vendor=NXP -pLPC824&amp;nbsp;&amp;nbsp;&amp;nbsp; -reset=vectreset -flash-driver=LPC800_32.cfx&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Where this one is the same for whichever device I select. And this command doesnt specify anywhere that it selects the specific device.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I then moved to the command line and tried to select a particular device but unable to succeed as the hid seems to be similar for both the devices. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I tried using the wire command and tried copying the serial number of the devices but still the same device was programmed again and again.&amp;nbsp; &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The command I used was&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;For one&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;C:\Users\elpk5\Documents\LPCXpresso_7.8.0_426\workspace\i2cTest\Debug\i2cTest.ax&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;f" -g -2&amp;nbsp; -vendor=NXP -pLPC824&amp;nbsp; --wire &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;\\?\hid#vid_0d28&amp;amp;pid_0204&amp;amp;mi_03#8&amp;amp;22e35216&amp;amp;0&amp;amp;0000#{4d1e55b2-f16f-11cf-88cb-001111000030}&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;For another&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;C:\Users\elpk5\Documents\LPCXpresso_7.8.0_426\workspace\i2cTest\Debug\i2cTest.ax&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;f" -g -2&amp;nbsp; -vendor=NXP -pLPC824&amp;nbsp; --wire \\?\hid#vid_0d28&amp;amp;pid_0204&amp;amp;mi_03#9&amp;amp;350bb73a&amp;amp;0&amp;amp;0000#{4d1e55b2-f16f-11cf-88cb-001111000030}&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Could you give me suggestions if I am making any mistake.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I want to connect both the devices to the same pc simultaneously and program them separately by selecting them individually.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I am attaching some of my screen shots.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks in Advance. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:52:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Issues-while-program-flash-multiple-device/m-p/573807#M21608</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:52:41Z</dc:date>
    </item>
    <item>
      <title>Re: Issues while program flash multiple device</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Issues-while-program-flash-multiple-device/m-p/573808#M21609</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by lpcxpresso-support on Wed Sep 09 14:32:44 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The LPCXpresso Flash Dialog does not support multiple probes. If it did, you would see the command line include a '-ProbeHandle=' argument. However, there's no reason why you can't do this from a command shell provided you know the parameter yourself. You can try adding:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;-ProbeHandle=1 or -ProbeHandle=2 to the command line&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks and regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;LPCXpresso Support&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:52:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Issues-while-program-flash-multiple-device/m-p/573808#M21609</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:52:41Z</dc:date>
    </item>
    <item>
      <title>Re: Issues while program flash multiple device</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Issues-while-program-flash-multiple-device/m-p/573809#M21610</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by partheepan on Thu Sep 10 05:01:49 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks for your reply.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Could you please let me know where could I find the parameters and could you please give me an example command line as it would be a great help.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:52:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Issues-while-program-flash-multiple-device/m-p/573809#M21610</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:52:42Z</dc:date>
    </item>
    <item>
      <title>Re: Issues while program flash multiple device</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Issues-while-program-flash-multiple-device/m-p/573810#M21611</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by lpcxpresso-support on Thu Sep 10 14:58:53 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;It's really not necessary to use the command-line interface. The Flash Dialog has a list box named "Extended Additional Options" where you can add the parameter I mentioned earlier. As far as determining which is probe 1 and which is probe 2, you can DFU the CMSIS-DAP probe (see boot_link2 script) to each probe in turn, and make note of the HID Path, or the Device Manager Device Instance Path.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;To view the connected probes in the Redlink Server using the command-line interface, start the Redlink Server using the command-line below. The ProbeList command will list the enumerated probes. Note in this case, probe 1 has booted the CMSIS-DAP bridge firmware image, and&amp;nbsp; probe 2 has booted the CMSIS-DAP non-bridge firmware image.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;C:\nxp\LPCXpresso_7.9.0_455\lpcxpresso\bin&amp;gt;redlinkserv.exe -commandline&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;redlink&amp;gt;probelist&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Index = 1&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Manufacturer = NXP Semiconductors&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Description = LPC-LINK2 CMSIS-DAP V5.112&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;VID:PID = 1FC9:0090&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Instance Object:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Path = \\?\hid#vid_1fc9&amp;amp;pid_0090&amp;amp;mi_00#8&amp;amp;ff48f8a&amp;amp;0&amp;amp;0000#{4d1e55b2-f16f-11cf-88cb-001111000030}&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Index = 2&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Manufacturer = NXP Semiconductors&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Description = LPC-LINK2 CMSIS-DAP V5.112 NB&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;VID:PID = 1FC9:0090&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Instance Object:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Path = \\?\hid#vid_1fc9&amp;amp;pid_0090&amp;amp;mi_00#a&amp;amp;13980cf4&amp;amp;0&amp;amp;0000#{4d1e55b2-f16f-11cf-88cb-001111000030&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;}&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;redlink&amp;gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks and regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;LPCXpresso Support&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:52:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Issues-while-program-flash-multiple-device/m-p/573810#M21611</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:52:43Z</dc:date>
    </item>
    <item>
      <title>Re: Issues while program flash multiple device</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Issues-while-program-flash-multiple-device/m-p/573811#M21612</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by partheepan on Fri Sep 11 04:19:28 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks for your reply.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I tried doing the probe list command and got the list. And went back to the flash dialog box and tried adding -ProbeHandle=1 and&amp;nbsp; -ProbeHandle=2 command to the Extended Additional Options. But it still flashes the same board again and again.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I then went back to command line and tried to do the same adding -ProbeHandle command but still not working.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have attached all the screen shots for what i did.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Please do help me to solve this problem.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks in advance. &lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:52:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Issues-while-program-flash-multiple-device/m-p/573811#M21612</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:52:43Z</dc:date>
    </item>
    <item>
      <title>Re: Issues while program flash multiple device</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Issues-while-program-flash-multiple-device/m-p/573812#M21613</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by partheepan on Mon Sep 21 03:48:15 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I still couldn't resolve this issue. Just wanted to know that are you still working on this issue.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:52:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Issues-while-program-flash-multiple-device/m-p/573812#M21613</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:52:44Z</dc:date>
    </item>
    <item>
      <title>Re: Issues while program flash multiple device</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Issues-while-program-flash-multiple-device/m-p/573813#M21614</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by lpcxpresso-support on Tue Sep 22 07:48:20 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;You didn't provide enough console output to determine where the trouble might be. For the time being please consider this as unsupported, and we'll investigate a fix in a future release.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks and regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;LPCXpresso Support&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:52:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Issues-while-program-flash-multiple-device/m-p/573813#M21614</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:52:44Z</dc:date>
    </item>
  </channel>
</rss>