<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LPC1769 LPCXpresso and USB example in LPCXpresso IDE</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1769-LPCXpresso-and-USB-example/m-p/573658#M21550</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Rob65 on Sat May 21 08:41:18 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Another way of getting 5V to your board is by soldering a wire between the SB-VBUS line of the LPC-Link and the Vin pin of the board - see attached photo.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Please note that this will also power the LPC-link when you connect the board through the USB-Uart or USB-Device connector, something you may not want to ...&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Rob&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 23:52:07 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T23:52:07Z</dc:date>
    <item>
      <title>LPC1769 LPCXpresso and USB example</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1769-LPCXpresso-and-USB-example/m-p/573656#M21548</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by JojoS on Sat May 21 08:01:58 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;dear LPC users, I'm new to the LPC's and still checking some examples. I use the Board from EmbeddedArtists together with their BaseBoard to connect Ethernet, USB and other. Some examples are running, but I got also some that were written for other hardware from CodeRed or Keil.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I was able to run the current FreeRTos 7.0.1 version by changing the code for the different phy hardware. Now I want to get a USB host running and found the Keil example 'usbmem'. But here I'm not successfull. The code compiles and I've set different breakpoints, but I get only an USB_Reset_Event when connecting an USB memory stick, no other events. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;What is missing? I checked the hardware drawings and set jumpers for terminating the USB lines, but then I get not even the reset event. I use only the USB host connector, the parallel USB device Interface is disconnected. The EA board has an output connected to a transistor to turn 3.3 V on the DP line, what should be done with this output? Keeping this line low changes nothing.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;What else can I check?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:52:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1769-LPCXpresso-and-USB-example/m-p/573656#M21548</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:52:06Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1769 LPCXpresso and USB example</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1769-LPCXpresso-and-USB-example/m-p/573657#M21549</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Rob65 on Sat May 21 08:26:00 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Did you connect an external 5V supply?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;You need to connect a 5V supply to Vin - a convenient way to do this is through the USB-UART bridge - I made the same problem when playing with the RGB LED, some peripherals need external 5V which is not supplied through the LPC-Link part of the board.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Also do not forget to insert the jumpers in J61 and do not use the USB device connector (X1, next to the USB-A connector) since these share the same USB signals.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Next thing to do is to use the correct program; usbmem is a memory device, not a host. Please download the lpc1768 sample applications from the Embedded Artists support site (&lt;/SPAN&gt;&lt;A href="http://http://www.embeddedartists.com/support/xpr/base/index.php"&gt;link&lt;/A&gt;&lt;SPAN&gt;) there you will find the usbhostlite application ready for the LPCXpresso environment.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;That should work.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Rob&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:52:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1769-LPCXpresso-and-USB-example/m-p/573657#M21549</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:52:06Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1769 LPCXpresso and USB example</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1769-LPCXpresso-and-USB-example/m-p/573658#M21550</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Rob65 on Sat May 21 08:41:18 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Another way of getting 5V to your board is by soldering a wire between the SB-VBUS line of the LPC-Link and the Vin pin of the board - see attached photo.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Please note that this will also power the LPC-link when you connect the board through the USB-Uart or USB-Device connector, something you may not want to ...&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Rob&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:52:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1769-LPCXpresso-and-USB-example/m-p/573658#M21550</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:52:07Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1769 LPCXpresso and USB example</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1769-LPCXpresso-and-USB-example/m-p/573659#M21551</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by JojoS on Sat May 21 08:50:54 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;thanks Rob, &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;yes power is supplied thru -x3 and nothing is connected to -x1. I had the other samples already and found the usbhostlite also. Now it reads my memory stick and reports FAT ok. This is really great stuff!&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:52:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1769-LPCXpresso-and-USB-example/m-p/573659#M21551</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:52:08Z</dc:date>
    </item>
  </channel>
</rss>