<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDEのトピックRe: EA Base Board &amp; MBED : I/O Problems</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/EA-Base-Board-MBED-I-O-Problems/m-p/573406#M21448</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by caprock on Wed Mar 31 11:00:46 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;No doubt that the EA code works but I may have a defective unit, either mbed or base. This is the reason for the post. Seems that my hardware is behaving differently from others.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;That is the only explanation that I can come up with why can't clear all 7-segments, and why when I write to each segment in bit order the results do not match. Simple test 7-segment: spi.write(0xbf) - bit 6 on my board this is the Decimal point but all docs say that the Decimal point is spi.write(0xdf) - bit 5.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I cannot understand the descrepancy but since I only have one base board&amp;nbsp; and one mbed I must reach out to others to confirm one way or another.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;In the meantime I have ordered an additional Base board and the LCPXpresso LCP1343 - perhaps this will help.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jun 2016 02:25:35 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-16T02:25:35Z</dc:date>
    <item>
      <title>EA Base Board &amp; MBED : I/O Problems</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/EA-Base-Board-MBED-I-O-Problems/m-p/573404#M21446</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by caprock on Tue Mar 30 15:31:10 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I have the Embedded Artists Base Board (EA-XPR-021) with the MBED installed and am having some difficulty getting certain interfaces to work. Chances are that I have mis-understood a pinout, but somethings just look questionable. And to top it off, support at Embedded Artists cannot seem to concur. Perhaps one of these two boards are responsible.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I have published my simple tests at: &lt;/SPAN&gt;&lt;A href="http://"&gt;http://mbed.org/users/caprock/programs/EA_SegIoTest/602vg/&lt;/A&gt;&lt;SPAN&gt; The test starts with the "Group Segments &amp;amp; RGB Led". Depress the Joystick to advance to "March Bits b0 =&amp;gt; b7". Depress the Joystick to advance to "March Segments SA =&amp;gt; SG, DP". (note: The EA board options are as set at the factory)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;At the moment I see three problems:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;1) The 7-segment display always has the lower right segment On.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;2) This 7-segment pinout and segent order does not seem to match the schematic. The schematic shows the display with a 180 degree rotation, placing the decimal point at the upper left. The published Rev A has b7 &amp;lt;- b0 as: FC.BAGED (correct rotation) but the actual segment order seems to be: b7 &amp;lt;- b0 as: F.EDGBAC (the period . is the Decimal Point). Another observation: the SPI/OLED interface is Ok.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;3) The RGB interface does not seem to work. (not reported yet) With the "Group Segments &amp;amp; RGB Led" test, I am writing 1: RGB_RED (0x01), 2: RGB_GREEN (0x04), 3: RGB_BLUE (0x02), 4: All (0x07). What I seem to get is: 1: Red, 2: none, 3: none, 4: Red + Blue&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;At the moment I am totally confused and would really appreciate someone with theses boards running the test program and reply with the results.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 02:25:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/EA-Base-Board-MBED-I-O-Problems/m-p/573404#M21446</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T02:25:34Z</dc:date>
    </item>
    <item>
      <title>Re: EA Base Board &amp; MBED : I/O Problems</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/EA-Base-Board-MBED-I-O-Problems/m-p/573405#M21447</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by brucesegal on Wed Mar 31 10:42:23 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;The demo software supplied by EA works with the baseboard and the lpc1114 or lpc1343 (i've tried both) correctly. At least the 7 segment display counts&amp;nbsp; and the RGB works. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I haven't looked closely at the code to see if the schematic differs from the code yet. Something else on the list of things to do. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I did write some test code to work with the RGB leds. I will try to find it and post it.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 02:25:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/EA-Base-Board-MBED-I-O-Problems/m-p/573405#M21447</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T02:25:35Z</dc:date>
    </item>
    <item>
      <title>Re: EA Base Board &amp; MBED : I/O Problems</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/EA-Base-Board-MBED-I-O-Problems/m-p/573406#M21448</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by caprock on Wed Mar 31 11:00:46 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;No doubt that the EA code works but I may have a defective unit, either mbed or base. This is the reason for the post. Seems that my hardware is behaving differently from others.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;That is the only explanation that I can come up with why can't clear all 7-segments, and why when I write to each segment in bit order the results do not match. Simple test 7-segment: spi.write(0xbf) - bit 6 on my board this is the Decimal point but all docs say that the Decimal point is spi.write(0xdf) - bit 5.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I cannot understand the descrepancy but since I only have one base board&amp;nbsp; and one mbed I must reach out to others to confirm one way or another.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;In the meantime I have ordered an additional Base board and the LCPXpresso LCP1343 - perhaps this will help.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 02:25:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/EA-Base-Board-MBED-I-O-Problems/m-p/573406#M21448</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T02:25:35Z</dc:date>
    </item>
    <item>
      <title>Re: EA Base Board &amp; MBED : I/O Problems</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/EA-Base-Board-MBED-I-O-Problems/m-p/573407#M21449</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by brucesegal on Wed Mar 31 12:07:40 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I understand.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I can say that the baseboard RGB leds are connected as documented in the manual and schematic. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;A program that toggles bits PIO1-2, PIO1-9, and PIO1-10 will toggle the various leds. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I may borrow an mbed from a friend and see whats up.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 02:25:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/EA-Base-Board-MBED-I-O-Problems/m-p/573407#M21449</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T02:25:36Z</dc:date>
    </item>
  </channel>
</rss>