<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDE中的主题 Configure SSP Clock</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/Configure-SSP-Clock/m-p/572955#M21236</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by andersonf on Wed May 25 05:29:31 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello I need help!&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;What is the maximum amount of SSP clock that can work with the LPC1343&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;72Mhz?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;SSP my clock is set to 4 MHz. Looking at the user manual data sheet &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;register Clock SSP0 Prescale Register - CPSDVSR is set to value 2.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;This value is 2 to 254 .. and the greater is my slowest clock. One value can not be set!&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Need to increase the clock SSP. which register / bit should I change?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks!&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Anderson&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 23:49:58 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T23:49:58Z</dc:date>
    <item>
      <title>Configure SSP Clock</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Configure-SSP-Clock/m-p/572955#M21236</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by andersonf on Wed May 25 05:29:31 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello I need help!&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;What is the maximum amount of SSP clock that can work with the LPC1343&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;72Mhz?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;SSP my clock is set to 4 MHz. Looking at the user manual data sheet &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;register Clock SSP0 Prescale Register - CPSDVSR is set to value 2.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;This value is 2 to 254 .. and the greater is my slowest clock. One value can not be set!&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Need to increase the clock SSP. which register / bit should I change?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks!&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Anderson&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:49:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Configure-SSP-Clock/m-p/572955#M21236</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:49:58Z</dc:date>
    </item>
    <item>
      <title>Re: Configure SSP Clock</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Configure-SSP-Clock/m-p/572956#M21237</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Ex-Zero on Wed May 25 05:55:45 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Take a look at LPC_SSP-&amp;gt;CR0 bit 8-15: SCR&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;SCR Serial Clock Rate. The number of prescaler-output clocks per bit on the bus, minus one. Given that CPSDVSR is the prescale divider, and the APB clock PCLK clocks the prescaler, the bit frequency is PCLK / (CPSDVSR × [SCR+1]).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;With:&lt;/SPAN&gt;&lt;BR /&gt;&lt;TABLE border="1"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD bgcolor="#cacaca"&gt; &lt;PRE&gt;
/* Set DSS data to 8-bit, Frame format SPI, CPOL = 0, CPHA = 0, and SCR 0*/
&amp;nbsp; LPC_SSP-&amp;gt;CR0 = 0x0007;
&lt;/PRE&gt; &lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;SPAN&gt;you should be able to run SSP up to 36MHz &lt;SPAN class="lia-unicode-emoji" title=":slightly_smiling_face:"&gt;&lt;LI-EMOJI id="lia_slightly-smiling-face" title=":slightly_smiling_face:"&gt;&lt;/LI-EMOJI&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Note: If you are using a standard LPC_SSP-&amp;gt;CR0 = 0x0707; your CLOCK is 72MHz /2 / 8 = 4.5MHz&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:49:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Configure-SSP-Clock/m-p/572956#M21237</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:49:58Z</dc:date>
    </item>
  </channel>
</rss>