<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Semihosting question in LPCXpresso IDE</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/Semihosting-question/m-p/572866#M21201</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by rjm on Thu Jan 22 07:11:56 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;&lt;SPAN&gt;According to &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fsupport.code-red-tech.com%2FCodeRedWiki%2FUsingPrintf" rel="nofollow" target="_blank"&gt;http://support.code-red-tech.com/CodeRedWiki/UsingPrintf&lt;/A&gt;&lt;SPAN&gt;, it is possible for the target, to read the host console via sscanf and even to open a file on the host.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Can I also redirect the output of the target MCU that appears in the host console to a file or pipe it to another program, e.g. a graphic visualiser - hence allowing to create live graphs.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 23:52:13 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T23:52:13Z</dc:date>
    <item>
      <title>Semihosting question</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Semihosting-question/m-p/572866#M21201</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by rjm on Thu Jan 22 07:11:56 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;&lt;SPAN&gt;According to &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fsupport.code-red-tech.com%2FCodeRedWiki%2FUsingPrintf" rel="nofollow" target="_blank"&gt;http://support.code-red-tech.com/CodeRedWiki/UsingPrintf&lt;/A&gt;&lt;SPAN&gt;, it is possible for the target, to read the host console via sscanf and even to open a file on the host.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Can I also redirect the output of the target MCU that appears in the host console to a file or pipe it to another program, e.g. a graphic visualiser - hence allowing to create live graphs.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:52:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Semihosting-question/m-p/572866#M21201</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:52:13Z</dc:date>
    </item>
    <item>
      <title>Re: Semihosting question</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Semihosting-question/m-p/572867#M21202</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by lpcxpresso-support on Thu Jan 22 07:39:53 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Please use the FAQ for LPCXpresso...&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.lpcware.com%2Fcontent%2Ffaq%2Flpcxpresso%2Fusing-printf" rel="nofollow" target="_blank"&gt;http://www.lpcware.com/content/faq/lpcxpresso/using-printf&lt;/A&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;No, you cannot redirect things written to the debug console. However, you can use fprintf() to write to a file on the host. Alternatively, as described in the above FAQ, you can retarget the output to another device, such as a UART. You could then read the UART with an application on the host.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:52:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Semihosting-question/m-p/572867#M21202</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:52:14Z</dc:date>
    </item>
  </channel>
</rss>