<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LPC2362 RAM size in LPCXpresso IDE</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC2362-RAM-size/m-p/572418#M20984</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by finfo on Mon May 31 12:23:14 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I have the following problem.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I am developing a prototype with an LPC2362.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;As Code Red writes they support this device I used it. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Now I am trying to implement a software. It uses a lot of RAM and some flash.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Now when you create a new project with the project wizard you come to the window you can see in the attached figure. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;This window shows especially the address where the RAM begins. This Ram is calles Ram32. But the size of it is about 0x2000 which is about 8kB. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;If you look in the Datasheet which you can download on: &lt;/SPAN&gt;&lt;A href="http://"&gt;http://www.nxp.com/#/pip/pip=&lt;/A&gt;&lt;SPAN&gt;[pip=LPC2361_62_4]|pp=[t=pip,i=LPC2361_62_4]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;you can see the LPC2362 definitely has 32 kBytes of Ram. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Now is my question is this a failure or do you have to buy the upgrade for this. And if it is a failure how can I manually change the RAM size. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;As the nowhere written down a limited Ram usage I think it must be a mistake. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;If you look in the memoy mapping in the Datasheet the adressrange for this device is 0x4000 0000 to 0x4000 7FFF which is 32 kBytes.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Maybe someone knows advice.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Florian&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 22:31:21 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T22:31:21Z</dc:date>
    <item>
      <title>LPC2362 RAM size</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC2362-RAM-size/m-p/572418#M20984</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by finfo on Mon May 31 12:23:14 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I have the following problem.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I am developing a prototype with an LPC2362.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;As Code Red writes they support this device I used it. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Now I am trying to implement a software. It uses a lot of RAM and some flash.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Now when you create a new project with the project wizard you come to the window you can see in the attached figure. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;This window shows especially the address where the RAM begins. This Ram is calles Ram32. But the size of it is about 0x2000 which is about 8kB. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;If you look in the Datasheet which you can download on: &lt;/SPAN&gt;&lt;A href="http://"&gt;http://www.nxp.com/#/pip/pip=&lt;/A&gt;&lt;SPAN&gt;[pip=LPC2361_62_4]|pp=[t=pip,i=LPC2361_62_4]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;you can see the LPC2362 definitely has 32 kBytes of Ram. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Now is my question is this a failure or do you have to buy the upgrade for this. And if it is a failure how can I manually change the RAM size. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;As the nowhere written down a limited Ram usage I think it must be a mistake. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;If you look in the memoy mapping in the Datasheet the adressrange for this device is 0x4000 0000 to 0x4000 7FFF which is 32 kBytes.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Maybe someone knows advice.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Florian&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:31:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC2362-RAM-size/m-p/572418#M20984</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:31:21Z</dc:date>
    </item>
    <item>
      <title>Re: LPC2362 RAM size</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC2362-RAM-size/m-p/572419#M20985</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by CodeRedSupport on Mon May 31 13:49:49 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;This is a mistake and will be fixed in the net release of LPCXpresso. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;You can manually define your linker scripts (based on the generated one) by following the knowledgebase entry:&lt;/SPAN&gt;&lt;BR /&gt;&lt;A href="http://"&gt;http://lpcxpresso.code-red-tech.com/LPCXpresso/node/31&lt;/A&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:31:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC2362-RAM-size/m-p/572419#M20985</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:31:22Z</dc:date>
    </item>
    <item>
      <title>Re: LPC2362 RAM size</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC2362-RAM-size/m-p/572420#M20986</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by finfo on Tue Jun 01 00:19:36 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Thank you. I got it working with that.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Florian&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:31:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC2362-RAM-size/m-p/572420#M20986</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:31:23Z</dc:date>
    </item>
  </channel>
</rss>