<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDE中的主题 Re: Programming bin's to LPC1768</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/Programming-bin-s-to-LPC1768/m-p/572309#M20948</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by CodeRedSupport on Fri Jun 04 14:57:24 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;The base address is where it is going to load your code. Assuming it is a standrard application this should be zero. A binary file is just that - binary data. It has no address information, so you have to tell it where to load.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Of course you can just give it the axf file, which contains all the address information, so in that case you wouldn't need to give anything else&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 22:31:10 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T22:31:10Z</dc:date>
    <item>
      <title>Programming bin's to LPC1768</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Programming-bin-s-to-LPC1768/m-p/572308#M20947</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by tecnosys on Fri Jun 04 09:02:36 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I've put a serial wire connector on a prototype board I've made, and thinking I should be able to program it with my LPCXPRESSO LPCLink. What should the base address be for the LPC1768?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;crt_emu_cm3_nxp -wire=winusb -pLPC1768 -flash-load=output.bin -load-base=0x???? &amp;lt;-- What base address should I be using here&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Info on LPCLINK command line programming&lt;/SPAN&gt;&lt;BR /&gt;&lt;A href="http://"&gt;http://lpcxpresso.code-red-tech.com/LPCXpresso/node/51&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Many Thanks&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Jason&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:31:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Programming-bin-s-to-LPC1768/m-p/572308#M20947</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:31:09Z</dc:date>
    </item>
    <item>
      <title>Re: Programming bin's to LPC1768</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Programming-bin-s-to-LPC1768/m-p/572309#M20948</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by CodeRedSupport on Fri Jun 04 14:57:24 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;The base address is where it is going to load your code. Assuming it is a standrard application this should be zero. A binary file is just that - binary data. It has no address information, so you have to tell it where to load.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Of course you can just give it the axf file, which contains all the address information, so in that case you wouldn't need to give anything else&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:31:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Programming-bin-s-to-LPC1768/m-p/572309#M20948</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:31:10Z</dc:date>
    </item>
  </channel>
</rss>