<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDEのトピックRe: Issue with DFU driver Windows 7</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/Issue-with-DFU-driver-Windows-7/m-p/571826#M20786</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by clcorbin on Wed Apr 09 16:12:46 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;One step forward, ....&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;So the LPC-Link2 showed up today.&amp;nbsp; The quick plug it in and see if the IDE can see it test worked out fine.&amp;nbsp; After the test, Windows recognized when the device was disconnected like it should.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;So on to the next test: I carefully cut the LPCXpresso 11C24 board apart at the link-target line.&amp;nbsp; I soldered a female pin header into the top of the LPC-Link2 and a mail pin header into the bottom of the target board at the 10 pin link-target connector.&amp;nbsp; After plugging in the target to the LPC-Link2 and connecting the LPC-Link2 to the USB port, the red LED on the LPC-Link2 comes on solid and the red LED on the target starts blinking like it should (it has one of the blink LED firmwares loaded from the one time I was able to get the original link to work!).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;When I tried to debug a different firmware, everything seems to boot and connect correctly, but then I get this error:&lt;/SPAN&gt;&lt;BR /&gt;&lt;TABLE border="1"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD bgcolor="#cacaca"&gt; &lt;PRE&gt;Error reported by sever (redlinkserv.exe):
RedlinkAPI: Wire Ack Fault - target connected?&lt;/PRE&gt; &lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The target has power, so I know VSS and VDD are connected correctly (powered from LPC-Link2), and so I ASSUME the other lines are also connected to the correct pins.&amp;nbsp; I've ohmed out the pins from the LPC-Link2 side to the target side of the connector and everything has continuity.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Just for fun, I've tried to enter debug mode without the target connected, but with the LPC-Link2 connected and I get a similar, but different error:&lt;/SPAN&gt;&lt;BR /&gt;&lt;TABLE border="1"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD bgcolor="#cacaca"&gt; &lt;PRE&gt;Error reported by sever (redlinkserv.exe):
RedlinkAPI: Wire Ack Fault - target connected?
Redlink Server will be restarted.
Please restart your debug session.&lt;/PRE&gt; &lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Any ideas on what I have screwed up at this point?&amp;nbsp; &lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 22:29:52 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T22:29:52Z</dc:date>
    <item>
      <title>Issue with DFU driver Windows 7</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Issue-with-DFU-driver-Windows-7/m-p/571821#M20781</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by clcorbin on Mon Apr 07 10:19:36 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Gents,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I've been going round and round with my LPCXpresso LPC11C24 with LPCXpresso 7.1.0.122.&amp;nbsp; Specifically, I can not connect to it.&amp;nbsp; When it is fist plugged in, the device is located and the DFU driver is loaded (and is in the device manager).&amp;nbsp; If I unplug it a this point, it will be removed from the device manager and the computer gives the normal USB disconnect tone.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;After I try to initialize the LPC-Link (either through the IDE by clicking debug, by clicking the "Boot Debug Probe" button or by following the Code Red command line diagnostics), I can not longer "remove it" from my system.&amp;nbsp; When I unplug it, it remains in the device manager and all the software acts the same no matter if it is plugged in or not: "device does not support download".&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;More importantly, it locks up USB enumeration on my system completely.&amp;nbsp; All USB devices that were plugged in prior to this work perfectly fine (the LPC-Link being the exception of course).&amp;nbsp; But any new USB device (say another USB mouse for example) will not enumerate and it will not work.&amp;nbsp; Plus, when I power the computer down, it hangs at shutting down.&amp;nbsp; I have to give the power button the 4 second salute to get it to power down.&amp;nbsp; Needless to say, on the next boot Windows reports it did not shut down properly.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have tried manually removing the driver and installing the driver in the LPCXpresso 7.1.0.122 Drivers folder using the pnputil from the command line.&amp;nbsp; I've tried the HID and winusb drivers (both through the IDE and the command line scripts).&amp;nbsp; I've updated the BIOS on my computer (Asus Z87-Plus based), on the USB controller chipset and updated all the drivers to the latest versions.&amp;nbsp; Nothing has made any difference what so ever.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;To REALLY piss me off, ONCE, I got the thing to connect and debug perfectly!&amp;nbsp; And no, I did not do anything differently at that time, as far as I can recall.&amp;nbsp; &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have two of these boards and they both work perfectly on my laptop, but both behave the same on this system.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Here is the log from one of the connection attempts:&lt;/SPAN&gt;&lt;BR /&gt;&lt;TABLE border="1"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD bgcolor="#cacaca"&gt; &lt;PRE&gt;*****************************************************
*** DFU LOG FILE ***
 Creation Time : C:\Users\Clint\AppData\Local\Temp\dfuApp8785148347567980203.log
*****************************************************


Open Device
Get Device Descriptor successful
Get Configuration Descriptor successful
DFU Get Status successful
---&amp;gt; DFUStatus: No error condition present.
---&amp;gt; DFUState: Device is operating in the DFU mode and is waiting for requests.

 Device Descriptor 
bLength: 0x12 
bDescriptorType: 0x01 
bcdUSB: 0x0200 
bDeviceClass: 0x00 
bDeviceSubClass: 0x00 
bDeviceProtocol: 0x00 
bMaxPacketSize0: 0x40 
idVendor: 0x0471 
idProduct: 0xdf55 
bcdDevice: 0x0001 
iManufacturer: 0x00 
iProduct: 0x00 
iSerialNumber: 0x00 
bNumConfigurations: 0x01 



DFU Get State successful
---&amp;gt; DFUState: Device is operating in the DFU mode and is waiting for requests.
Download Block Nb 0 (2048 Bytes)
DFU Get State successful
---&amp;gt; DFUState: Device has received a block and is waiting for the host to solicit the status via DFU_GETSTATUS.
DFU Get Status successful
---&amp;gt; DFUStatus: No error condition present.
---&amp;gt; DFUState: Device is processing a download operation. Expecting DFU_DNLOAD requests.
Download Block Nb 1 (2048 Bytes)
DFU Get State successful
---&amp;gt; DFUState: Device has received a block and is waiting for the host to solicit the status via DFU_GETSTATUS.
DFU Get Status successful
---&amp;gt; DFUStatus: No error condition present.
---&amp;gt; DFUState: Device is processing a download operation. Expecting DFU_DNLOAD requests.
Download Block Nb 2 (2048 Bytes)
DFU Get State successful
---&amp;gt; DFUState: Device has received a block and is waiting for the host to solicit the status via DFU_GETSTATUS.
DFU Get Status successful
---&amp;gt; DFUStatus: No error condition present.
---&amp;gt; DFUState: Device is processing a download operation. Expecting DFU_DNLOAD requests.
Download Block Nb 3 (2048 Bytes)
DFU Get State successful
---&amp;gt; DFUState: Device has received a block and is waiting for the host to solicit the status via DFU_GETSTATUS.
DFU Get Status successful
---&amp;gt; DFUStatus: No error condition present.
---&amp;gt; DFUState: Device is processing a download operation. Expecting DFU_DNLOAD requests.
Download Block Nb 4 (2048 Bytes)
DFU Get State successful
---&amp;gt; DFUState: Device has received a block and is waiting for the host to solicit the status via DFU_GETSTATUS.
DFU Get Status successful
---&amp;gt; DFUStatus: No error condition present.
---&amp;gt; DFUState: Device is processing a download operation. Expecting DFU_DNLOAD requests.
Download Block Nb 5 (2048 Bytes)
DFU Get State successful
---&amp;gt; DFUState: Device has received a block and is waiting for the host to solicit the status via DFU_GETSTATUS.
DFU Get Status successful
---&amp;gt; DFUStatus: No error condition present.
---&amp;gt; DFUState: Device is processing a download operation. Expecting DFU_DNLOAD requests.
Download Block Nb 6 (2048 Bytes)
DFU Get State successful
---&amp;gt; DFUState: Device has received a block and is waiting for the host to solicit the status via DFU_GETSTATUS.
DFU Get Status successful
---&amp;gt; DFUStatus: No error condition present.
---&amp;gt; DFUState: Device is processing a download operation. Expecting DFU_DNLOAD requests.
Download Block Nb 7 (2048 Bytes)
DFU Get State successful
---&amp;gt; DFUState: Device has received a block and is waiting for the host to solicit the status via DFU_GETSTATUS.
DFU Get Status successful
---&amp;gt; DFUStatus: No error condition present.
---&amp;gt; DFUState: Device is processing a download operation. Expecting DFU_DNLOAD requests.
Download Block Nb 8 (2048 Bytes)
DFU Get State successful
---&amp;gt; DFUState: Device has received a block and is waiting for the host to solicit the status via DFU_GETSTATUS.
DFU Get Status successful
---&amp;gt; DFUStatus: No error condition present.
---&amp;gt; DFUState: Device is processing a download operation. Expecting DFU_DNLOAD requests.
Download Block Nb 9 (2048 Bytes)
DFU Get State successful
---&amp;gt; DFUState: Device has received a block and is waiting for the host to solicit the status via DFU_GETSTATUS.
DFU Get Status successful
---&amp;gt; DFUStatus: No error condition present.
---&amp;gt; DFUState: Device is processing a download operation. Expecting DFU_DNLOAD requests.
Download Block Nb 10 (2048 Bytes)
DFU Get State successful
---&amp;gt; DFUState: Device has received a block and is waiting for the host to solicit the status via DFU_GETSTATUS.
DFU Get Status successful
---&amp;gt; DFUStatus: No error condition present.
---&amp;gt; DFUState: Device is processing a download operation. Expecting DFU_DNLOAD requests.
Download Block Nb 11 (2048 Bytes)
DFU Get State successful
---&amp;gt; DFUState: Device has received a block and is waiting for the host to solicit the status via DFU_GETSTATUS.
DFU Get Status successful
---&amp;gt; DFUStatus: No error condition present.
---&amp;gt; DFUState: Device is processing a download operation. Expecting DFU_DNLOAD requests.
Download Block Nb 12 (2048 Bytes)
DFU Get State successful
---&amp;gt; DFUState: Device has received a block and is waiting for the host to solicit the status via DFU_GETSTATUS.
DFU Get Status successful
---&amp;gt; DFUStatus: No error condition present.
---&amp;gt; DFUState: Device is processing a download operation. Expecting DFU_DNLOAD requests.
Download Block Nb 13 (2048 Bytes)
DFU Get State successful
---&amp;gt; DFUState: Device has received a block and is waiting for the host to solicit the status via DFU_GETSTATUS.
DFU Get Status successful
---&amp;gt; DFUStatus: No error condition present.
---&amp;gt; DFUState: Device is processing a download operation. Expecting DFU_DNLOAD requests.
Download Block Nb 14 (520 Bytes)
DFU Get State successful
---&amp;gt; DFUState: Device has received a block and is waiting for the host to solicit the status via DFU_GETSTATUS.
DFU Get Status successful
---&amp;gt; DFUStatus: No error condition present.
---&amp;gt; DFUState: Device is processing a download operation. Expecting DFU_DNLOAD requests.
Download Block Nb 15 (0 Bytes)
DFU Get State successful
---&amp;gt; DFUState: Device has received the final block of firmware from the host and is waiting for receipt of DFU_GETSTATUS to begin the Manifestation phase; or device has completed the Manifestation phase and is waiting for receipt of DFU_GETSTATUS. (Devices that can enter this state after the Manifestation phase set bmAttributes bit bitManifestationTolerant to 1.)
DFU Get Status successful
---&amp;gt; DFUStatus: No error condition present.
---&amp;gt; DFUState: Device has programmed its memories and is waiting for a USB reset or a power on reset. (Devices that must enter this state clear bitManifestationTolerant to 0.)
Device Reset after Download successful
Close Device



 *** END OF FILE *** &lt;/PRE&gt; &lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Any attempts to connect a second time after a boot gives me the "device does not support download" message and the log file is completely empty.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm at a lose.&amp;nbsp; Any ideas on what to try next?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Clint&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:29:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Issue-with-DFU-driver-Windows-7/m-p/571821#M20781</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:29:49Z</dc:date>
    </item>
    <item>
      <title>Re: Issue with DFU driver Windows 7</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Issue-with-DFU-driver-Windows-7/m-p/571822#M20782</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by clcorbin on Mon Apr 07 10:22:25 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Also, the errors listed after the connection failed is &lt;/SPAN&gt;&lt;BR /&gt;&lt;TABLE border="1"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD bgcolor="#cacaca"&gt; &lt;PRE&gt;Timeout waiting for LPC-Link (WinUSB) or RDB-Link to initialize.


Timeout waiting for LPC-Link (WinUSB) or RDB-Link to initialize.

&amp;nbsp; 
&amp;nbsp; at com.crt.debugcommon.emulator.common.AbstractCommonBootableProbe.booter(Unknown Source)
&amp;nbsp; at com.crt.debugcommon.emulator.common.AbstractCommonBootableProbe.access$1(Unknown Source)
&amp;nbsp; at com.crt.debugcommon.emulator.common.AbstractCommonBootableProbe$2.run(Unknown Source)
&amp;nbsp; at org.eclipse.jface.operation.ModalContext$ModalContextThread.run(ModalContext.java:121)
&lt;/PRE&gt; &lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:29:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Issue-with-DFU-driver-Windows-7/m-p/571822#M20782</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:29:50Z</dc:date>
    </item>
    <item>
      <title>Re: Issue with DFU driver Windows 7</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Issue-with-DFU-driver-Windows-7/m-p/571823#M20783</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by lpcxpresso-support on Mon Apr 07 10:49:06 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Try different USB ports. If you are using USB3, you may need to upgrade the firmware for you USB3 ports. Alternatively, use USB2 ports.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:29:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Issue-with-DFU-driver-Windows-7/m-p/571823#M20783</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:29:50Z</dc:date>
    </item>
    <item>
      <title>Re: Issue with DFU driver Windows 7</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Issue-with-DFU-driver-Windows-7/m-p/571824#M20784</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by clcorbin on Mon Apr 07 11:01:55 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I've tried multiple ports, both USB3 and USB2.&amp;nbsp; They all act the same.&amp;nbsp; As was originally posted, the USB firmware has already been updated to the latest release with no change in behavior.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:29:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Issue-with-DFU-driver-Windows-7/m-p/571824#M20784</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:29:51Z</dc:date>
    </item>
    <item>
      <title>Re: Issue with DFU driver Windows 7</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Issue-with-DFU-driver-Windows-7/m-p/571825#M20785</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by clcorbin on Tue Apr 08 08:43:33 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Last night I also found which ports on my Asus Z87-Plus are not driven off the north bridge but are from a stand alone chip and tried one of those ports.&amp;nbsp; And got the exact same results.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;At this point, I suspect something just isn't right with Window's USB stack or drivers.&amp;nbsp; I ordered a Segger J-Link and an LPC-Linkv2 yesterday, so I'll have a bit more diagnostic tool available in a few days.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Clint&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:29:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Issue-with-DFU-driver-Windows-7/m-p/571825#M20785</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:29:52Z</dc:date>
    </item>
    <item>
      <title>Re: Issue with DFU driver Windows 7</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Issue-with-DFU-driver-Windows-7/m-p/571826#M20786</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by clcorbin on Wed Apr 09 16:12:46 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;One step forward, ....&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;So the LPC-Link2 showed up today.&amp;nbsp; The quick plug it in and see if the IDE can see it test worked out fine.&amp;nbsp; After the test, Windows recognized when the device was disconnected like it should.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;So on to the next test: I carefully cut the LPCXpresso 11C24 board apart at the link-target line.&amp;nbsp; I soldered a female pin header into the top of the LPC-Link2 and a mail pin header into the bottom of the target board at the 10 pin link-target connector.&amp;nbsp; After plugging in the target to the LPC-Link2 and connecting the LPC-Link2 to the USB port, the red LED on the LPC-Link2 comes on solid and the red LED on the target starts blinking like it should (it has one of the blink LED firmwares loaded from the one time I was able to get the original link to work!).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;When I tried to debug a different firmware, everything seems to boot and connect correctly, but then I get this error:&lt;/SPAN&gt;&lt;BR /&gt;&lt;TABLE border="1"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD bgcolor="#cacaca"&gt; &lt;PRE&gt;Error reported by sever (redlinkserv.exe):
RedlinkAPI: Wire Ack Fault - target connected?&lt;/PRE&gt; &lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The target has power, so I know VSS and VDD are connected correctly (powered from LPC-Link2), and so I ASSUME the other lines are also connected to the correct pins.&amp;nbsp; I've ohmed out the pins from the LPC-Link2 side to the target side of the connector and everything has continuity.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Just for fun, I've tried to enter debug mode without the target connected, but with the LPC-Link2 connected and I get a similar, but different error:&lt;/SPAN&gt;&lt;BR /&gt;&lt;TABLE border="1"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD bgcolor="#cacaca"&gt; &lt;PRE&gt;Error reported by sever (redlinkserv.exe):
RedlinkAPI: Wire Ack Fault - target connected?
Redlink Server will be restarted.
Please restart your debug session.&lt;/PRE&gt; &lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Any ideas on what I have screwed up at this point?&amp;nbsp; &lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:29:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Issue-with-DFU-driver-Windows-7/m-p/571826#M20786</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:29:52Z</dc:date>
    </item>
    <item>
      <title>Re: Issue with DFU driver Windows 7</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Issue-with-DFU-driver-Windows-7/m-p/571827#M20787</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by clcorbin on Wed Apr 09 18:25:34 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;To make things even more interesting, I WAS able to successfully debug (multiple times no less) this 11C24 board using the J-Link.&amp;nbsp; I did have to use the LPC-Link2 to provide 3.3V power and I used jumper wires to connect the same 9 pin (not 10 like I thought before) connector to the J-Link's 20 pin cable.&amp;nbsp; It worked perfectly even if it WAS a mess on the desk!&amp;nbsp; &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;After scratching my head a bit, I decided to give the LPC-LINK2 another try.&amp;nbsp; This time, I used the SAME jumper wires used with the J-Link to connect to J6 on the LPC-Link2.&amp;nbsp; They worked with the J-Link, so they should work with the LPC-Link2 I would think.&amp;nbsp; I also pulled up the LPCXpresso 11C24 board schematic and the LPC-LINK2 schematic to make SURE that the LPCXpresso target connectors were wired exactly the same between boards (they were).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;And the silly thing still doesn't work.&amp;nbsp; &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The next test was to apply flux to the header in J6 and resolder each of the terminals in case one is not soldered in well.&amp;nbsp; I know the header on the target works because it works with the J-Link.&amp;nbsp; And again, needless to say, there was no difference.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Now I'm starting to wonder if I don't have any issue with the LPC-Link2.&amp;nbsp; The transceiver perhaps?&amp;nbsp; Does anyone have any suggestions on what to scope out to test this?&amp;nbsp; What's the chance it was bad from the start?&amp;nbsp; I would assume it was tested before it was packaged.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Clint&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:29:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Issue-with-DFU-driver-Windows-7/m-p/571827#M20787</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:29:53Z</dc:date>
    </item>
  </channel>
</rss>