<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDE中的主题 LPCXpresso 1343 work alone</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPCXpresso-1343-work-alone/m-p/570601#M20197</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by frnkyan on Wed Mar 23 12:11:07 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I have a LPCXpresso 1343, works good with the USB cable connecting PC. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Now I need to let the "target side" work alone (without USB-link) for temperature test. ( "target side" is the right half of the board, without the LPC-link located at left half of the board , just the LPC1343 and the 12Mhz Xtal and a led) &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I did cut 8 wires connecting left and right half of the board (J4) and have 3.3VDC from an external power supply connecting pin-2 and GND connecting pin-16. the progam that runs is the blinky from the examples.This code makes the LED blinking.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;When I power on, 3.3VDC went to the board but I don't see the LED blinking. the current of the external power supply displays 0.1amp&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;After that, I re-connect these 8 wires, put the board back to the origunal connection to PC throught USB cable, LED blinks again.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Should I have a push button or something to start?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Please help&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 22:29:47 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T22:29:47Z</dc:date>
    <item>
      <title>LPCXpresso 1343 work alone</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPCXpresso-1343-work-alone/m-p/570601#M20197</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by frnkyan on Wed Mar 23 12:11:07 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I have a LPCXpresso 1343, works good with the USB cable connecting PC. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Now I need to let the "target side" work alone (without USB-link) for temperature test. ( "target side" is the right half of the board, without the LPC-link located at left half of the board , just the LPC1343 and the 12Mhz Xtal and a led) &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I did cut 8 wires connecting left and right half of the board (J4) and have 3.3VDC from an external power supply connecting pin-2 and GND connecting pin-16. the progam that runs is the blinky from the examples.This code makes the LED blinking.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;When I power on, 3.3VDC went to the board but I don't see the LED blinking. the current of the external power supply displays 0.1amp&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;After that, I re-connect these 8 wires, put the board back to the origunal connection to PC throught USB cable, LED blinks again.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Should I have a push button or something to start?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Please help&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:29:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPCXpresso-1343-work-alone/m-p/570601#M20197</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:29:47Z</dc:date>
    </item>
    <item>
      <title>Re: LPCXpresso 1343 work alone</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPCXpresso-1343-work-alone/m-p/570602#M20198</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Ex-Zero on Wed Mar 23 13:50:43 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Not sure which pins we are talking about :)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;A href="http://"&gt;http://www.embeddedartists.com/products/lpcxpresso/LPCXpressoLPC1343revA.pdf&lt;/A&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Sheet 5 shows correct connection:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;J1-1 GND&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;J1-28 +3.3V&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;After connecting target board to VCC it should blink immediately.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Power consumption should be &amp;lt; 20mA.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:29:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPCXpresso-1343-work-alone/m-p/570602#M20198</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:29:48Z</dc:date>
    </item>
    <item>
      <title>Re: LPCXpresso 1343 work alone</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPCXpresso-1343-work-alone/m-p/570603#M20199</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by larryvc on Wed Mar 23 14:27:06 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Little typo. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;J4-16&amp;nbsp; =&amp;nbsp;&amp;nbsp; J6-1&amp;nbsp;&amp;nbsp;&amp;nbsp; GNDX&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; GND&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;J4-2&amp;nbsp;&amp;nbsp;&amp;nbsp; =&amp;nbsp;&amp;nbsp; J6-28&amp;nbsp; VIO_3V3X&amp;nbsp;&amp;nbsp; +3.3V&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Power should be ok.&amp;nbsp; I don't have this board so can't verify.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Try J6-1 and J6-28 for Gnd and 3.3V as Zero meant.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:29:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPCXpresso-1343-work-alone/m-p/570603#M20199</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:29:48Z</dc:date>
    </item>
  </channel>
</rss>