<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDEのトピックDALI SDK - for Linux?</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/DALI-SDK-for-Linux/m-p/570472#M20146</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by sglpc.2015 on Sun Apr 26 01:53:48 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I see that DALI SDK 2.0 zip file contains a Windows .exe. Is there a DALI SDK for Linux?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jun 2016 02:23:00 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-16T02:23:00Z</dc:date>
    <item>
      <title>DALI SDK - for Linux?</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/DALI-SDK-for-Linux/m-p/570472#M20146</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by sglpc.2015 on Sun Apr 26 01:53:48 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I see that DALI SDK 2.0 zip file contains a Windows .exe. Is there a DALI SDK for Linux?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 02:23:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/DALI-SDK-for-Linux/m-p/570472#M20146</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T02:23:00Z</dc:date>
    </item>
    <item>
      <title>Re: DALI SDK - for Linux?</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/DALI-SDK-for-Linux/m-p/570473#M20147</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by sglpc.2015 on Mon Apr 27 21:18:21 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Please advise if I should move this query to another forum.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;If this is not the right one, which is ?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 02:23:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/DALI-SDK-for-Linux/m-p/570473#M20147</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T02:23:01Z</dc:date>
    </item>
    <item>
      <title>Re: DALI SDK - for Linux?</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/DALI-SDK-for-Linux/m-p/570474#M20148</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Pat on Mon May 04 01:43:08 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;The DALI SDK2.0 is a self installing .exe for windows. The micro controller sources that are being installed (unzipped) by this file can be used with LPCXPresso under Linux.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Best is to install the SDK on a windows machine and copy the complete installed tree (typically at C:\nxp\lighting\DALI_SDK_v2.0 ) to a Linux host.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;This should allow development on a Linux machine.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;As background: once installed it provides the following on the windows PC:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;-&amp;nbsp; documentation (application notes, user manual, schematics)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;-&amp;nbsp; example PC GUI to use with the DALI master board. (Using .NET)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;-&amp;nbsp; source code of master and slave microcontroller boards&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;-&amp;nbsp; source code of PC GUI&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 02:23:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/DALI-SDK-for-Linux/m-p/570474#M20148</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T02:23:01Z</dc:date>
    </item>
  </channel>
</rss>