<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic IDE 5.2.2 Debugger Issue -- Show Stopper in LPCXpresso IDE</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/IDE-5-2-2-Debugger-Issue-Show-Stopper/m-p/570169#M20005</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by MikeSimmonds on Wed Apr 24 06:06:42 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;[FONT=Tahoma][SIZE=2][Win XP Pro/SP3 32 Bit]&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;It seems that the latest debugger is not keeping accurate track of its hardware&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;breakpoints?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;On the screenshot, it is clear that no bp's are set, the hardware FPB has no&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;bp's enabled, but the debugger claims that no breakpoint resources are free.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Additional background:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I had a [I]single[/I] bp (at LoadModule). This was called 3 times and in each call I:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;did 2 'run to line' followed by an F6 (step over 'bl' call) and continue.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I noticed that the memory view on the FPB registes showed all 6 bp registers active.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;However, a single F5 (step into) cleared these in the memory view.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I then attempted to 'run to line' in a "C" file and the error depicted showed up.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I think the debugger is at fault, but I you say not so, how can we remove these&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;bp's that the IDE thinks it, presumably, has to insert during the 'continue' phase&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;so that a new run to line bp can be inserted?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;NB: The forum has reduced the size of the attachment, but (in FireFox with an&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;addon) I can zoom the image enough to see the text. Ask if you need the original&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;jpg attached as a zip.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards, Mike&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;[/SIZE][/FONT]&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jun 2016 01:04:52 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-16T01:04:52Z</dc:date>
    <item>
      <title>IDE 5.2.2 Debugger Issue -- Show Stopper</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/IDE-5-2-2-Debugger-Issue-Show-Stopper/m-p/570169#M20005</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by MikeSimmonds on Wed Apr 24 06:06:42 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;[FONT=Tahoma][SIZE=2][Win XP Pro/SP3 32 Bit]&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;It seems that the latest debugger is not keeping accurate track of its hardware&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;breakpoints?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;On the screenshot, it is clear that no bp's are set, the hardware FPB has no&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;bp's enabled, but the debugger claims that no breakpoint resources are free.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Additional background:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I had a [I]single[/I] bp (at LoadModule). This was called 3 times and in each call I:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;did 2 'run to line' followed by an F6 (step over 'bl' call) and continue.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I noticed that the memory view on the FPB registes showed all 6 bp registers active.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;However, a single F5 (step into) cleared these in the memory view.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I then attempted to 'run to line' in a "C" file and the error depicted showed up.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I think the debugger is at fault, but I you say not so, how can we remove these&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;bp's that the IDE thinks it, presumably, has to insert during the 'continue' phase&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;so that a new run to line bp can be inserted?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;NB: The forum has reduced the size of the attachment, but (in FireFox with an&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;addon) I can zoom the image enough to see the text. Ask if you need the original&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;jpg attached as a zip.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards, Mike&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;[/SIZE][/FONT]&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 01:04:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/IDE-5-2-2-Debugger-Issue-Show-Stopper/m-p/570169#M20005</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T01:04:52Z</dc:date>
    </item>
    <item>
      <title>Re: IDE 5.2.2 Debugger Issue -- Show Stopper</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/IDE-5-2-2-Debugger-Issue-Show-Stopper/m-p/570170#M20006</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by MikeSimmonds on Wed Apr 24 07:21:25 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;[FONT=Tahoma][SIZE=2]I added the update to the wrong thread.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Please see &lt;/SPAN&gt;&lt;A href="http://"&gt;http://knowledgebase.nxp.com/showthread.php?t=4446&lt;/A&gt;&lt;SPAN&gt; post 2&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Sorry for my ineptitude.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[/SIZE][/FONT]&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 01:04:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/IDE-5-2-2-Debugger-Issue-Show-Stopper/m-p/570170#M20006</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T01:04:53Z</dc:date>
    </item>
  </channel>
</rss>