<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic usbd_lib_cdc LPCXpresso 1769 in LPCXpresso IDE</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/usbd-lib-cdc-LPCXpresso-1769/m-p/569049#M19550</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by capstone on Mon Jun 23 13:33:50 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Previously posted in the LPC Open forum and closed as in the wrong forum.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;LPC Open v2.10/LPCXpresso v7.2.0/Windows 7/64&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Has anyone had success connecting the USB with usbd_lib_cdc built on the Xpresso Base Board?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;If so, will you please share the details/changes/file.inf etc.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Also, I have a question about the underlying library usbd_175x_6x_lib: is there any reason that this library would not support an alternate build for the Code Red RDB1768R2 Development Board?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks!&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;STRONG&gt;Resolved.&lt;/STRONG&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;After much searching I have resolved the connection problem.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;First of all, it appears that the USB_CONNECT is not biased by the v2.10&amp;nbsp; lpc_board_nxp_lpcxpresso_1769/board.c/Board_USBD_Init procedure to make the usb visible to the host.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Adding this line provides the bias to the D+ signal line:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;TABLE border="1"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD bgcolor="#cacaca"&gt; &lt;PRE&gt;
void Board_USBD_Init(uint32_t port)
{
/* set a bias to this pin to enable the host system to detect and begin enumeration */
Chip_IOCON_PinMux(LPC_IOCON, 2, 9, IOCON_MODE_INACT, IOCON_FUNC1);&amp;nbsp; /* USB_CONNECT */
&lt;/PRE&gt; &lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.lpcware.com%2Fcontent%2Fforum%2Flpcxpresso-lpc1769-usbcdc-example" rel="nofollow noopener noreferrer" target="_blank"&gt;http://www.lpcware.com/content/forum/lpcxpresso-lpc1769-usbcdc-example&lt;/A&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The next may or may not be an issue, depending on the target system. There was no INF file matching the requirements of &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;VID = 0x1FC9 and PID = 0x83 found in the lpc-ucom-vcom.inf file. The following link provides several development interface files:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.lpcware.com%2Fcontent%2Fnxpfile%2Flpcopen-software-platform-usbd-library-drivers-windows" rel="nofollow noopener noreferrer" target="_blank"&gt;http://www.lpcware.com/content/nxpfile/lpcopen-software-platform-usbd-library-drivers-windows&lt;/A&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;All's well now for the lpc_board_nxp_lpcxpresso_1769 build.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 22:26:27 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T22:26:27Z</dc:date>
    <item>
      <title>usbd_lib_cdc LPCXpresso 1769</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/usbd-lib-cdc-LPCXpresso-1769/m-p/569049#M19550</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by capstone on Mon Jun 23 13:33:50 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Previously posted in the LPC Open forum and closed as in the wrong forum.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;LPC Open v2.10/LPCXpresso v7.2.0/Windows 7/64&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Has anyone had success connecting the USB with usbd_lib_cdc built on the Xpresso Base Board?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;If so, will you please share the details/changes/file.inf etc.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Also, I have a question about the underlying library usbd_175x_6x_lib: is there any reason that this library would not support an alternate build for the Code Red RDB1768R2 Development Board?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks!&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;STRONG&gt;Resolved.&lt;/STRONG&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;After much searching I have resolved the connection problem.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;First of all, it appears that the USB_CONNECT is not biased by the v2.10&amp;nbsp; lpc_board_nxp_lpcxpresso_1769/board.c/Board_USBD_Init procedure to make the usb visible to the host.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Adding this line provides the bias to the D+ signal line:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;TABLE border="1"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD bgcolor="#cacaca"&gt; &lt;PRE&gt;
void Board_USBD_Init(uint32_t port)
{
/* set a bias to this pin to enable the host system to detect and begin enumeration */
Chip_IOCON_PinMux(LPC_IOCON, 2, 9, IOCON_MODE_INACT, IOCON_FUNC1);&amp;nbsp; /* USB_CONNECT */
&lt;/PRE&gt; &lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.lpcware.com%2Fcontent%2Fforum%2Flpcxpresso-lpc1769-usbcdc-example" rel="nofollow noopener noreferrer" target="_blank"&gt;http://www.lpcware.com/content/forum/lpcxpresso-lpc1769-usbcdc-example&lt;/A&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The next may or may not be an issue, depending on the target system. There was no INF file matching the requirements of &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;VID = 0x1FC9 and PID = 0x83 found in the lpc-ucom-vcom.inf file. The following link provides several development interface files:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.lpcware.com%2Fcontent%2Fnxpfile%2Flpcopen-software-platform-usbd-library-drivers-windows" rel="nofollow noopener noreferrer" target="_blank"&gt;http://www.lpcware.com/content/nxpfile/lpcopen-software-platform-usbd-library-drivers-windows&lt;/A&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;All's well now for the lpc_board_nxp_lpcxpresso_1769 build.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:26:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/usbd-lib-cdc-LPCXpresso-1769/m-p/569049#M19550</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:26:27Z</dc:date>
    </item>
  </channel>
</rss>