<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDE中的主题 RTC on LPC812</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/RTC-on-LPC812/m-p/568902#M19473</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by teekaytk on Mon Feb 11 16:01:33 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;dear all&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I am converting from PIC so I am not very sure what would be the best way to implement a real time clock in LPC 812. I'll have a 32khz external oscillator producing a 32khz square wave. When working with PIC all I had to do was connect it to one of the clk inputs to timer and then I could use it as interrupt every 32K cycles (one second). After the interrupt had been dealt with the PIC went to sleep so saved me a lot of power.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Can Something similar be done in LPC. I may have a GPS signal from time to time that I may be able to use to reset the clock if it has drifted a bit..&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks for your help.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 23:46:50 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T23:46:50Z</dc:date>
    <item>
      <title>RTC on LPC812</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/RTC-on-LPC812/m-p/568902#M19473</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by teekaytk on Mon Feb 11 16:01:33 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;dear all&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I am converting from PIC so I am not very sure what would be the best way to implement a real time clock in LPC 812. I'll have a 32khz external oscillator producing a 32khz square wave. When working with PIC all I had to do was connect it to one of the clk inputs to timer and then I could use it as interrupt every 32K cycles (one second). After the interrupt had been dealt with the PIC went to sleep so saved me a lot of power.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Can Something similar be done in LPC. I may have a GPS signal from time to time that I may be able to use to reset the clock if it has drifted a bit..&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks for your help.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:46:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/RTC-on-LPC812/m-p/568902#M19473</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:46:50Z</dc:date>
    </item>
    <item>
      <title>Re: RTC on LPC812</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/RTC-on-LPC812/m-p/568903#M19474</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Ex-Zero on Mon Feb 11 16:21:26 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Of course you can keep your LPC busy with 32k/sec Interrupts :rolleyes:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;But you could also invest 1€ in good old MCP79410 with real RTC and 1 sec output :)&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:46:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/RTC-on-LPC812/m-p/568903#M19474</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:46:51Z</dc:date>
    </item>
    <item>
      <title>Re: RTC on LPC812</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/RTC-on-LPC812/m-p/568904#M19475</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by teekaytk on Mon Feb 11 16:49:42 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;good idea..it may increase the product cost a bit but may make life easier at development time&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;thanks&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:46:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/RTC-on-LPC812/m-p/568904#M19475</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:46:52Z</dc:date>
    </item>
  </channel>
</rss>