<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDEのトピックRe: LPC-Link connection problems</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC-Link-connection-problems/m-p/568751#M19409</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by dmayer on Wed May 09 10:21:01 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;How could it be possibile, that it runs flawlessly as root, if there is a lib missing? I'll try to find out if there is a 32-bit libusb-1.0, but your explanation seems strange to me...&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;EDIT:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[B]I installed the 32-bit libusb-1.0 from &lt;/SPAN&gt;&lt;A href="http://http://www.ubuntuupdates.org/package/core/precise/main/base/libusb-1.0-0"&gt;here&lt;/A&gt;&lt;SPAN&gt; and it seemes to work [/B]now. I dont have a target to verify definitely but im quite shure this was the problem.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thank you VERY much gogamoga! I really appreciate your help!! :)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;PS: Still dont understand how there could miss libs, that only cause a failure for normal users, but not for root.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jun 2016 01:00:01 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-16T01:00:01Z</dc:date>
    <item>
      <title>LPC-Link connection problems</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC-Link-connection-problems/m-p/568708#M19366</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by mbeale on Thu Apr 19 20:52:06 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Environment: System Linux Ubuntu (Lucid) 10.04 (IA64), Debugging using Eclipse/Code-red (LPCXpresso_4.2.2_238_Linux-x86) with a LPC-Link JTAG interface pcb, Micro LPC1225.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Debugger reports following error:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;No emulator/board available.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;This could be because it is unpowered, disconnected or already in use&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;However am able to debug without problems while running as sudo (root). This problem has occurred with earlier versions of Code-red compilers. Appears to be an issue with permissions. Have tried other tip from the forum without success.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Any suggestions? Don't like running applications as super user unless I absolutely have to.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;malcolm&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:59:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC-Link-connection-problems/m-p/568708#M19366</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T00:59:33Z</dc:date>
    </item>
    <item>
      <title>Re: LPC-Link connection problems</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC-Link-connection-problems/m-p/568709#M19367</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by researchinnovation on Thu Apr 19 21:25:16 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi....!!!&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;1.)Sometime for a board we use two USB cable connection, one for power and other one UART. So if we use single cable then it may not provide sufficient power to the board.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;2.) Sometime we use different emulator and select different Emulator/hardware/processor/boardmodel(for example LPC1114/302) in the IDE(For example LPC1114/301) which does not match.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;3.)Sometime we do not have Windows host/driver or FTDI driver or driver of right version according to PC(windows xp/vista, ubuntu etc.).&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;4.) Sometime if IDE is in running mode and want to run again then also it can show this error.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;5.) Sometime Reset in the registers happen continuously .&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Anyway..Just try. It might help you.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks &amp;amp; Regards ...:)&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:59:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC-Link-connection-problems/m-p/568709#M19367</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T00:59:34Z</dc:date>
    </item>
    <item>
      <title>Re: LPC-Link connection problems</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC-Link-connection-problems/m-p/568710#M19368</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by CodeRedSupport on Fri Apr 20 00:15:11 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;This sounds like a permissions problem.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Accessing low-level USB drivers in Linux requires root access. When LPCXpresso is installed, it correctly sets the Debug drivers to run with root privileges. If these have been lost, then this explains your issue. To fix:&lt;/SPAN&gt;&lt;BR /&gt;&lt;TABLE border="1"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD bgcolor="#cacaca"&gt; &lt;PRE&gt;
cd /usr/local/lpcxpresso&amp;lt;version&amp;gt;/lpcxpresso/bin
sudo chown root crt_emu* dfu-util
sudo chgrp root crt_emu* dfu-util
sudo chmod 6755 crt_emu* dfu-util 
&lt;/PRE&gt; &lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;BR /&gt;&lt;SPAN&gt;This will restore the Debug drivers to their installed state.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:59:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC-Link-connection-problems/m-p/568710#M19368</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T00:59:34Z</dc:date>
    </item>
    <item>
      <title>Re: LPC-Link connection problems</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC-Link-connection-problems/m-p/568711#M19369</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by mbeale on Sun Apr 22 17:47:36 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: CodeRedSupport&lt;/STRONG&gt;&lt;BR /&gt;This sounds like a permissions problem.&lt;BR /&gt;&lt;BR /&gt;Accessing low-level USB drivers in Linux requires root access. When LPCXpresso is installed, it correctly sets the Debug drivers to run with root privileges. If these have been lost, then this explains your issue. To fix:&lt;BR /&gt;&lt;TABLE border="1"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD bgcolor="#cacaca"&gt; &lt;PRE&gt;
cd /usr/local/lpcxpresso&amp;lt;version&amp;gt;/lpcxpresso/bin
sudo chown root crt_emu* dfu-util
sudo chgrp root crt_emu* dfu-util
sudo chmod 6755 crt_emu* dfu-util 
&lt;/PRE&gt; &lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;BR /&gt;This will restore the Debug drivers to their installed state.&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi SM,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks for the feedback, tried your suggestion above but still same results (unable to find emulator). Please note I did check the file permissions for the dfu-util and crt_emu* (1 + 6 files) and they were all correctly set to 'root' privileges.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Reiterating, debug works fine when I run LPCXpresso as 'sudo'.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;A point to note, after the initial installation of LPCXpresso_4.2.2_238_Linux-x86 I was able to run and debug without problems as a standard user. This issue occurred the next day after the machine had been shut down and rebooted. It appears some other file necessary for debug operation has been set with incorrect privileges.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Any suggestions?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;malcolm&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:59:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC-Link-connection-problems/m-p/568711#M19369</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T00:59:35Z</dc:date>
    </item>
    <item>
      <title>Re: LPC-Link connection problems</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC-Link-connection-problems/m-p/568712#M19370</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by gogamoga on Tue Apr 24 19:57:39 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Unplug your LPCXpresso, plug it back,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Check permissions on usb device:&lt;/SPAN&gt;&lt;BR /&gt;&lt;TABLE border="1"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD bgcolor="#cacaca"&gt; &lt;PRE&gt;sudo lsusb | sed -n -e 's/bus \(.*\) device \(.*\):.*0471:df55.*/\/dev\/bus\/usb\/\1\/\2/Ip' | xargs ls -lha&lt;/PRE&gt; &lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Should read something like:&lt;/SPAN&gt;&lt;BR /&gt;&lt;TABLE border="1"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD bgcolor="#cacaca"&gt; &lt;PRE&gt;crw-rw-r-- 1 root usb 189, 4 Apr 25 05:40 /dev/bus/usb/001/005&lt;/PRE&gt; &lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;You might need to add yourself to usb group to fix this issue&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;P.S just noticed you are on (IA64), might be and issue with 32bit libs.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;check your libs with this:&lt;/SPAN&gt;&lt;BR /&gt;&lt;TABLE border="1"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD bgcolor="#cacaca"&gt; &lt;PRE&gt;ldconfig -p | sed -n -e 's/.* \(.*libusb\.so.*\)/\1/Ip' | xargs file -L&lt;/PRE&gt; &lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;and if you dont see any 32bit libusb, possible solution might be in this thread: &lt;/SPAN&gt;&lt;A href="http://http://knowledgebase.nxp.com/showthread.php?t=3144" rel="nofollow noopener noreferrer" target="_blank"&gt;http://knowledgebase.nxp.com/showthread.php?t=3144&lt;/A&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:59:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC-Link-connection-problems/m-p/568712#M19370</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T00:59:35Z</dc:date>
    </item>
    <item>
      <title>Re: LPC-Link connection problems</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC-Link-connection-problems/m-p/568713#M19371</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by mbeale on Wed Apr 25 19:03:32 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: gogamoga&lt;/STRONG&gt;&lt;BR /&gt;Unplug your LPCXpresso, plug it back,&lt;BR /&gt;Check permissions on usb device:&lt;BR /&gt;&lt;TABLE border="1"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD bgcolor="#cacaca"&gt; &lt;PRE&gt;sudo lsusb | sed -n -e 's/bus \(.*\) device \(.*\):.*0471:df55.*/\/dev\/bus\/usb\/\1\/\2/Ip' | xargs ls -lha&lt;/PRE&gt; &lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;BR /&gt;&lt;BR /&gt;Should read something like:&lt;BR /&gt;&lt;TABLE border="1"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD bgcolor="#cacaca"&gt; &lt;PRE&gt;crw-rw-r-- 1 root usb 189, 4 Apr 25 05:40 /dev/bus/usb/001/005&lt;/PRE&gt; &lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;BR /&gt;&lt;BR /&gt;You might need to add yourself to usb group to fix this issue&lt;BR /&gt;&lt;BR /&gt;P.S just noticed you are on (IA64), might be and issue with 32bit libs.&lt;BR /&gt;check your libs with this:&lt;BR /&gt;&lt;TABLE border="1"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD bgcolor="#cacaca"&gt; &lt;PRE&gt;ldconfig -p | sed -n -e 's/.* \(.*libusb\.so.*\)/\1/Ip' | xargs file -L&lt;/PRE&gt; &lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;BR /&gt;&lt;BR /&gt;and if you dont see any 32bit libusb, possible solution might be in this thread: &lt;A href="http://http://knowledgebase.nxp.com/showthread.php?t=3144" rel="nofollow noopener noreferrer" target="_blank"&gt;http://knowledgebase.nxp.com/showthread.php?t=3144&lt;/A&gt;&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi Gogamoga,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;First thanks for the feedback...&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;1. Ran the first long command string from your post and the results looked okay, they're listed below&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;crw-rw-r-- 1 root root 189, 132 2012-04-26 08:22 /dev/bus/usb/002/005&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;2. With reference to adding myself to the USB group - added myself to uucp group, and retired but no luck. Do I need to logout and back in order for uucp changes to be recognized by the system?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;3. 2 command give an error but didn't explore further, the command string appeared to be correct though.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;4. Looked at the 32bit libs reference towards end of your post, the libusb-1.0.so.0 is in the /lib directory, or rather a symlink to it is.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I did notice there was some discussion about using Ubuntu 12, I should be upgrading the system to the new 12.04 on 26 when the distribution is officially released and will try again, see what happens. Have read that lib hell is addressed in the new version.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Till then am continuing debug as sudo, if you have any other input I'll give it a go. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Again, your assistance is much appreciated.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;malcolm&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:59:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC-Link-connection-problems/m-p/568713#M19371</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T00:59:36Z</dc:date>
    </item>
    <item>
      <title>Re: LPC-Link connection problems</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC-Link-connection-problems/m-p/568714#M19372</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by gogamoga on Wed Apr 25 23:37:00 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Unplug, plug back, run this as normal user and post the results:&lt;/SPAN&gt;&lt;BR /&gt;&lt;TABLE border="1"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD bgcolor="#cacaca"&gt; &lt;PRE&gt;cd /usr/local/lpcxpresso&amp;lt;version&amp;gt;/lpcxpresso/bin
./dfu-util -d 0x471:0xdf55 -c 0 -t 2048 -R -D LPCXpressoWIN.enc&lt;/PRE&gt; &lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;SPAN&gt;If the result reads something like that:&lt;/SPAN&gt;&lt;BR /&gt;&lt;TABLE border="1"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD bgcolor="#cacaca"&gt; &lt;PRE&gt;dfu-util - (C) 2007-2008 by OpenMoko Inc.
This program is Free Software and has ABSOLUTELY NO WARRANTY

Opening USB Device 0x0471:0xdf55...
Claiming USB DFU Runtime Interface...
Cannot claim interface: could not claim interface 0: Operation not permitted&lt;/PRE&gt; &lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;SPAN&gt;You are clearly dont have SUID on dfu-util, fix it with this:&lt;/SPAN&gt;&lt;BR /&gt;&lt;TABLE border="1"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD bgcolor="#cacaca"&gt; &lt;PRE&gt;sudo chmod +s dfu-util&lt;/PRE&gt; &lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;SPAN&gt;If the output of dfu-util looks ok then try this:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;TABLE border="1"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD bgcolor="#cacaca"&gt; &lt;PRE&gt;./crt_emu_cm3_nxp -info-emu -wire=winusb&lt;/PRE&gt; &lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;SPAN&gt;crt_emu_cm3_nxp output should read something like:&lt;/SPAN&gt;&lt;BR /&gt;&lt;TABLE border="1"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD bgcolor="#cacaca"&gt; &lt;PRE&gt;Ni: LPCXpresso Debug Driver v4.0 (Mar 25 2012 14:25:27)
1 Emulators available:
0. LPCLINK_1_1&amp;nbsp;&amp;nbsp;&amp;nbsp; LPC-Link Driver LINUX32 v1.1 (Code Red - LPCXpresso)&lt;/PRE&gt; &lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;SPAN&gt;If you have this output there is no reason for lpcxpresso not to debug as normal user, but if it still doesnt work, then last solution - add udev rules:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;First, make sure that you are in plugdev group, if not -&amp;nbsp; add yourself :&lt;/SPAN&gt;&lt;BR /&gt;&lt;TABLE border="1"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD bgcolor="#cacaca"&gt; &lt;PRE&gt; sudo usermod -a -G plugdev `whoami`&lt;/PRE&gt; &lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;SPAN&gt;[COLOR=Red]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;***Note: you need to restart X to make group addition take effect[/COLOR]&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Then, run this:&lt;/SPAN&gt;&lt;BR /&gt;&lt;TABLE border="1"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD bgcolor="#cacaca"&gt; &lt;PRE&gt;sudo sh -c 'echo "# Rules for LPCXpresso DevBoard
SUBSYSTEM==\"usb\", ATTRS{idVendor}==\"0471\", ATTRS{idProduct}==\"df55\", MODE=\"0664\", GROUP=\"plugdev\"
SUBSYSTEM==\"usb\", ATTRS{idVendor}==\"1fc9\", ATTRS{idProduct}==\"0009\", MODE=\"0664\", GROUP=\"plugdev\"" &amp;gt; /etc/udev/rules.d/80-lpcxpresso.rules'
sudo restart udev&lt;/PRE&gt; &lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;SPAN&gt;Unplug, Plug back and run:&lt;/SPAN&gt;&lt;BR /&gt;&lt;TABLE border="1"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD bgcolor="#cacaca"&gt; &lt;PRE&gt;sudo lsusb | sed -n -e 's/bus \(.*\) device \(.*\):.*0471:df55.*/\/dev\/bus\/usb\/\1\/\2/Ip' | xargs ls -lha&lt;/PRE&gt; &lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;SPAN&gt;This should read something like: &lt;/SPAN&gt;&lt;TABLE border="1"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD bgcolor="#cacaca"&gt; &lt;PRE&gt;crw-rw-r-- 1 root plugdev 189, 145 2012-04-26 17:35 /dev/bus/usb/002/018&lt;/PRE&gt; &lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;SPAN&gt;[COLOR=Red]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;***Notice the crw-rw-r-- permissions and plugdev group[/COLOR]&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;This should make it work, no matter if dfu-util is SUID or not&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I cant think of anything else permission related that could go wrong there.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;P.S &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;How many versions of LPCXpresso you have installed?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:59:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC-Link-connection-problems/m-p/568714#M19372</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T00:59:37Z</dc:date>
    </item>
    <item>
      <title>Re: LPC-Link connection problems</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC-Link-connection-problems/m-p/568715#M19373</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by mbeale on Wed May 02 20:10:07 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: gogamoga&lt;/STRONG&gt;&lt;BR /&gt;Unplug, plug back, run this as normal user and post the results:&lt;BR /&gt;&lt;TABLE border="1"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD bgcolor="#cacaca"&gt; &lt;PRE&gt;cd /usr/local/lpcxpresso&amp;lt;version&amp;gt;/lpcxpresso/bin
./dfu-util -d 0x471:0xdf55 -c 0 -t 2048 -R -D LPCXpressoWIN.enc&lt;/PRE&gt; &lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;If the result reads something like that:&lt;BR /&gt;&lt;TABLE border="1"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD bgcolor="#cacaca"&gt; &lt;PRE&gt;dfu-util - (C) 2007-2008 by OpenMoko Inc.
This program is Free Software and has ABSOLUTELY NO WARRANTY

Opening USB Device 0x0471:0xdf55...
Claiming USB DFU Runtime Interface...
Cannot claim interface: could not claim interface 0: Operation not permitted&lt;/PRE&gt; &lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;You are clearly dont have SUID on dfu-util, fix it with this:&lt;BR /&gt;&lt;TABLE border="1"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD bgcolor="#cacaca"&gt; &lt;PRE&gt;sudo chmod +s dfu-util&lt;/PRE&gt; &lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;If the output of dfu-util looks ok then try this:&lt;BR /&gt;&lt;BR /&gt;&lt;TABLE border="1"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD bgcolor="#cacaca"&gt; &lt;PRE&gt;./crt_emu_cm3_nxp -info-emu -wire=winusb&lt;/PRE&gt; &lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;crt_emu_cm3_nxp output should read something like:&lt;BR /&gt;&lt;TABLE border="1"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD bgcolor="#cacaca"&gt; &lt;PRE&gt;Ni: LPCXpresso Debug Driver v4.0 (Mar 25 2012 14:25:27)
1 Emulators available:
0. LPCLINK_1_1&amp;nbsp;&amp;nbsp;&amp;nbsp; LPC-Link Driver LINUX32 v1.1 (Code Red - LPCXpresso)&lt;/PRE&gt; &lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;If you have this output there is no reason for lpcxpresso not to debug as normal user, but if it still doesnt work, then last solution - add udev rules:&lt;BR /&gt;&lt;BR /&gt;First, make sure that you are in plugdev group, if not -&amp;nbsp; add yourself :&lt;BR /&gt;&lt;TABLE border="1"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD bgcolor="#cacaca"&gt; &lt;PRE&gt; sudo usermod -a -G plugdev `whoami`&lt;/PRE&gt; &lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;[COLOR=Red]&lt;BR /&gt;***Note: you need to restart X to make group addition take effect[/COLOR]&lt;BR /&gt;&lt;BR /&gt;Then, run this:&lt;BR /&gt;&lt;TABLE border="1"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD bgcolor="#cacaca"&gt; &lt;PRE&gt;sudo sh -c 'echo "# Rules for LPCXpresso DevBoard
SUBSYSTEM==\"usb\", ATTRS{idVendor}==\"0471\", ATTRS{idProduct}==\"df55\", MODE=\"0664\", GROUP=\"plugdev\"
SUBSYSTEM==\"usb\", ATTRS{idVendor}==\"1fc9\", ATTRS{idProduct}==\"0009\", MODE=\"0664\", GROUP=\"plugdev\"" &amp;gt; /etc/udev/rules.d/80-lpcxpresso.rules'
sudo restart udev&lt;/PRE&gt; &lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;Unplug, Plug back and run:&lt;BR /&gt;&lt;TABLE border="1"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD bgcolor="#cacaca"&gt; &lt;PRE&gt;sudo lsusb | sed -n -e 's/bus \(.*\) device \(.*\):.*0471:df55.*/\/dev\/bus\/usb\/\1\/\2/Ip' | xargs ls -lha&lt;/PRE&gt; &lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;This should read something like: &lt;TABLE border="1"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD bgcolor="#cacaca"&gt; &lt;PRE&gt;crw-rw-r-- 1 root plugdev 189, 145 2012-04-26 17:35 /dev/bus/usb/002/018&lt;/PRE&gt; &lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;[COLOR=Red]&lt;BR /&gt;***Notice the crw-rw-r-- permissions and plugdev group[/COLOR]&lt;BR /&gt;&lt;BR /&gt;This should make it work, no matter if dfu-util is SUID or not&lt;BR /&gt;I cant think of anything else permission related that could go wrong there.&lt;BR /&gt;&lt;BR /&gt;P.S &lt;BR /&gt;How many versions of LPCXpresso you have installed?&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi Gogamoga,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Ok, before I feedback on your suggestions, I've made some system changes but the results appear similar.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;New OS Environment: Ubuntu Unity 12.04 LTS (64Bit)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Workstation Hardware: Dell Precision M6500 (unchanged from previous posts)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Clean install of Ubuntu Unity 12.04 LTS, installed LPCXpresso_4.2.2_238_Linux-X86, JTAG LPC-Link, target same as before.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;After install debug works fine as normal user.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Reboot machine, unable to debug as user (same problem as earlier), works fine as 'sudo'.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;With regard to your suggestions.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Closed LPCXpresso Eclipse, unplug LPC-Link and reconnected, output of first command follows:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;cd /usr/local/lpcxpresso&amp;lt;version&amp;gt;/lpcxpresso/bin&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;./dfu-util -d 0x471:0xdf55 -c 0 -t 2048 -R -D LPCXpressoWIN.enc&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;dfu-util - (C) 2007-2008 by OpenMoko Inc.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;This program is Free Software and has ABSOLUTELY NO WARRANTY&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Opening USB Device 0x0471:0xdf55...&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Claiming USB DFU Runtime Interface...&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Determining device status: state = dfuIDLE, status = 0&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;WARNING: Runtime device already in DFU state ?!?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Found Runtime: [0x0471:0xdf55] devnum=4, cfg=0, intf=0, alt=0, name="UNDEFINED"&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Claiming USB DFU Interface...&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Setting Alternate Setting ...&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Determining device status: state = dfuIDLE, status = 0&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;dfuIDLE, continuing&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Transfer Size = 0x0800&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;LPCXpressoWin.enc: No such file or directory&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Now if I startup LPCXpresso as standard user and attempt debug which fails as expected, I notice the USB ID of the device changed. The new ID is:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Running the same command as above produces the following results.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;dfu-util - (C) 2007-2008 by OpenMoko Inc.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;This program is Free Software and has ABSOLUTELY NO WARRANTY&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;No DFU capable USB device found&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Before I run the "sudo chmod +s dfu-util" command I check the permissions on dfu-util, they are correctly set to root, both the owner and group. Didn't run the command as I don't think it would have any effect.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Next command (note this is after attempting to debug in LPCXpresso, the result is the same if I unplug the LPC-Link and reconnect it, obviously the dfu-util was supposed to change the USB ID, so it no surprise)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;./crt_emu_cm3_nxp -info-emu -wire=winusb&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Ni: LPCXpresso Debug Driver v4.0 (Mar 25 2012 14:25:27)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;0 Emulators available:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Next "sudo usermod -a -G plugdev `whoami`". Added myself to the plugdev group through Ubuntu's group management applet instead of using command line.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Okay, now the long shell command to create the "80-lpcxpresso.rules" file in the udev/rules.d directory. I took the short cut and running gedit under sudo created a file with the name and copied your strings to it, and restarted udev as indicated on the last line. Note - no file of this name existed in the directory, should there have been one?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Finally, unplugged the device and plugged it back in and ran:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;sudo lsusb | sed -n -e 's/bus \(.*\) device \(.*\):.*0471:df55.*/\/dev\/bus\/usb\/\1\/\2/Ip' | xargs ls -lha&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;crw-rw-r-- 1 root root 189, 137 May&amp;nbsp; 3 10:51 /dev/bus/usb/002/010&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Restarted LPCXpresso as normal user and attempted debug but failed with same error.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I appreciate the time you've spent on looking at this problem. Just thought I'd provide the feedback so that anyone else with the same issue might find it helpful and if you're somehow connected with the LPCXpresso development project it might be useful feedback. I can continue embedded development using sudo until this is worked out.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm still not clear why debug always works fine the first time LPCXpresso is installed but fails thereafter when the machine is rebooted.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanx&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Malcolm&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:59:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC-Link-connection-problems/m-p/568715#M19373</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T00:59:38Z</dc:date>
    </item>
    <item>
      <title>Re: LPC-Link connection problems</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC-Link-connection-problems/m-p/568716#M19374</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by gogamoga on Wed May 02 21:23:29 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: mbeale&lt;/STRONG&gt;&lt;BR /&gt;...&lt;BR /&gt;cd /usr/local/lpcxpresso&amp;lt;version&amp;gt;/lpcxpresso/bin&lt;BR /&gt;./dfu-util -d 0x471:0xdf55 -c 0 -t 2048 -R -D LPCXpressoWIN.enc&lt;BR /&gt;&lt;BR /&gt;dfu-util - (C) 2007-2008 by OpenMoko Inc.&lt;BR /&gt;This program is Free Software and has ABSOLUTELY NO WARRANTY&lt;BR /&gt;&lt;BR /&gt;Opening USB Device 0x0471:0xdf55...&lt;BR /&gt;Claiming USB DFU Runtime Interface...&lt;BR /&gt;Determining device status: state = dfuIDLE, status = 0&lt;BR /&gt;WARNING: Runtime device already in DFU state ?!?&lt;BR /&gt;Found Runtime: [0x0471:0xdf55] devnum=4, cfg=0, intf=0, alt=0, name="UNDEFINED"&lt;BR /&gt;Claiming USB DFU Interface...&lt;BR /&gt;Setting Alternate Setting ...&lt;BR /&gt;Determining device status: state = dfuIDLE, status = 0&lt;BR /&gt;dfuIDLE, continuing&lt;BR /&gt;Transfer Size = 0x0800&lt;BR /&gt;LPCXpressoWin.enc: No such file or directory &lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;my input reads: LPCXpresso[COLOR=Red]WIN[/COLOR].enc your input reads: LPCXpresso[COLOR=Red]Win[/COLOR].enc&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;notice the LOWERCASE part of LPCXpressoW[COLOR=Red]in[/COLOR].enc ???&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Those things matter on linux - file names are case sensitive.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: &lt;/STRONG&gt;&lt;BR /&gt;...&lt;BR /&gt;Finally, unplugged the device and plugged it back in and ran:&lt;BR /&gt;sudo lsusb | sed -n -e 's/bus \(.*\) device \(.*\):.*0471:df55.*/\/dev\/bus\/usb\/\1\/\2/Ip' | xargs ls -lha&lt;BR /&gt;&lt;BR /&gt;crw-rw-r-- 1 root [COLOR=Red]root[/COLOR] 189, 137 May&amp;nbsp; 3 10:51 /dev/bus/usb/002/010&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Again, part marked red is a group. It is clearly seen that its not plugdev but root&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Which means - you have messed something with udev rules, which means again, you as a member of plugdev has no right to write to the device and here is your permission issue.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The reason is:&lt;/SPAN&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: &lt;/STRONG&gt;&lt;BR /&gt;...&lt;BR /&gt;Okay, now the long shell command to create the "80-lpcxpresso.rules" file in the udev/rules.d directory. I took the short cut and running gedit under sudo created a file with the name and copied your strings to it, and restarted udev as indicated on the last line. Note - no file of this name existed in the directory, should there have been one?&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;you either copy/paste the code that i gave, or edit with your editor, but!!!! remove the backslashes from quotes, which means, if you see '[COLOR=red]\"[/COLOR]' and edit the rules file with the editor you should replace it with '[COLOR=red]"[/COLOR]', or simplier copy/paste my input (this is the real shortcut lol)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Try again, fixing the issues i pointed out.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;If you still want to use the gedit, put this into rules file:&amp;nbsp; 80-lpcxpresso.rules&lt;/SPAN&gt;&lt;BR /&gt;&lt;TABLE border="1"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD bgcolor="#cacaca"&gt; &lt;PRE&gt;
# Rules for LPCXpresso DevBoard
SUBSYSTEM=="usb", ATTRS{idVendor}=="0471", ATTRS{idProduct}=="df55", MODE="0664", GROUP="plugdev"
SUBSYSTEM=="usb", ATTRS{idVendor}=="1fc9", ATTRS{idProduct}=="0009", MODE="0664", GROUP="plugdev"
&lt;/PRE&gt; &lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;and dont forget to restart udev&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;PS.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The reason i wrote the commands i wrote in the previous post is to really give you a way to use console and not to rely on ubuntu gui.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Console is power. Do not rely on the gui. Read howtos and learn basic commands, this is linux after all, not windows.&amp;nbsp; This is one of the things that annoys me in UBUNTU.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:59:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC-Link-connection-problems/m-p/568716#M19374</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T00:59:39Z</dc:date>
    </item>
    <item>
      <title>Re: LPC-Link connection problems</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC-Link-connection-problems/m-p/568717#M19375</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by researchinnovation on Wed May 02 21:28:33 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Excellent...!!!&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Good work...!!!:)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Keep it up.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:59:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC-Link-connection-problems/m-p/568717#M19375</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T00:59:39Z</dc:date>
    </item>
    <item>
      <title>Re: LPC-Link connection problems</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC-Link-connection-problems/m-p/568718#M19376</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by CodeRedSupport on Thu May 03 02:53:55 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I can confirm that we have installed LPCXpresso on Ubuntu 12.04 in both 32-bit and 64-bit and have found no issues at all - everything works exactly as expected. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Note that running when on 64-bit version, you need to install the ia32 libraries:&lt;/SPAN&gt;&lt;BR /&gt;&lt;TABLE border="1"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD bgcolor="#cacaca"&gt; &lt;PRE&gt;
sudo apt-get install ia32-libs-multiarch:i386
&lt;/PRE&gt; &lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Apart from that, these were completely cleans installs with no other components added.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:59:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC-Link-connection-problems/m-p/568718#M19376</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T00:59:40Z</dc:date>
    </item>
    <item>
      <title>Re: LPC-Link connection problems</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC-Link-connection-problems/m-p/568719#M19377</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by gogamoga on Thu May 03 03:08:02 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;He has it working as root so its not lib32 issues - its clearly permissions issue. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;CodeRed should consider udev rules instead of suid root binaries in next release (IMHO)&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:59:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC-Link-connection-problems/m-p/568719#M19377</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T00:59:40Z</dc:date>
    </item>
    <item>
      <title>Re: LPC-Link connection problems</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC-Link-connection-problems/m-p/568720#M19378</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by CodeRedSupport on Thu May 03 04:31:59 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;This is something we have been investigating for a while and are&amp;nbsp; currently testing. Perhaps you would like to beta test these rules?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;[LIST]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[*]download and unzip the attachment&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[*]copy the unzipped file to /etc/udev/rules.d&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[*]restart the udev service (sudo service udev restart)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[/LIST]&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;These rules will make any of the supported devices world-write when attached. It will also automatically boot LPC-Link&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:59:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC-Link-connection-problems/m-p/568720#M19378</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T00:59:41Z</dc:date>
    </item>
    <item>
      <title>Re: LPC-Link connection problems</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC-Link-connection-problems/m-p/568721#M19379</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by gogamoga on Thu May 03 04:56:00 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;if you are going to use codered udev rules, make sure you remove the previous rule file you created&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:59:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC-Link-connection-problems/m-p/568721#M19379</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T00:59:42Z</dc:date>
    </item>
    <item>
      <title>Re: LPC-Link connection problems</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC-Link-connection-problems/m-p/568722#M19380</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by MacGyverQue on Thu May 03 08:14:21 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: CodeRedSupport&lt;/STRONG&gt;&lt;BR /&gt;I can confirm that we have installed LPCXpresso on Ubuntu 12.04 in both 32-bit and 64-bit and have found no issues at all - everything works exactly as expected. &lt;BR /&gt;&lt;BR /&gt;Note that running when on 64-bit version, you need to install the ia32 libraries:&lt;BR /&gt;&lt;TABLE border="1"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD bgcolor="#cacaca"&gt; &lt;PRE&gt;
sudo apt-get install ia32-libs-multiarch:i386
&lt;/PRE&gt; &lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;Apart from that, these were completely cleans installs with no other components added.&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;** Sorry to Thread Jack But.... **&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm really happy to hear that there is hope for running LPCXpresso on Ubuntu 12, but I upgraded from 11 to 12 and am now running into licensing issues. Any suggestion? I posted a thread to the same effect.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:59:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC-Link-connection-problems/m-p/568722#M19380</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T00:59:42Z</dc:date>
    </item>
    <item>
      <title>Re: LPC-Link connection problems</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC-Link-connection-problems/m-p/568723#M19381</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by CodeRedSupport on Thu May 03 09:21:52 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Did you try deleting the license files and reactivating? /usr/share/LPCXpresso&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;We have found and fixed the issue you reported with the parse error, and that will be made available in the next release. However, is mentioned in your other post, Red Suite uses a completely different licensing system which is unaffected by this issue.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:59:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC-Link-connection-problems/m-p/568723#M19381</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T00:59:43Z</dc:date>
    </item>
    <item>
      <title>Re: LPC-Link connection problems</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC-Link-connection-problems/m-p/568724#M19382</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by mbeale on Thu May 03 18:04:07 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: MacGyverQue&lt;/STRONG&gt;&lt;BR /&gt;** Sorry to Thread Jack But.... **&lt;BR /&gt;I'm really happy to hear that there is hope for running LPCXpresso on Ubuntu 12, but I upgraded from 11 to 12 and am now running into licensing issues. Any suggestion? I posted a thread to the same effect.&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Yes, I encountered the same debug license limit problem too, but did what CodeRedSupport suggested (delete license file and reactivate) and the issue cleared.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:59:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC-Link-connection-problems/m-p/568724#M19382</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T00:59:43Z</dc:date>
    </item>
    <item>
      <title>Re: LPC-Link connection problems</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC-Link-connection-problems/m-p/568725#M19383</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by gogamoga on Fri May 04 01:34:05 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Did you fix the permission issue?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:59:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC-Link-connection-problems/m-p/568725#M19383</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T00:59:44Z</dc:date>
    </item>
    <item>
      <title>Re: LPC-Link connection problems</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC-Link-connection-problems/m-p/568726#M19384</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by mbeale on Fri May 04 02:55:23 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi gogamoga&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: gogamoga&lt;/STRONG&gt;&lt;BR /&gt;my input reads: LPCXpresso[COLOR=Red]WIN[/COLOR].enc your input reads: LPCXpresso[COLOR=Red]Win[/COLOR].enc&lt;BR /&gt;&lt;BR /&gt;notice the LOWERCASE part of LPCXpressoW[COLOR=Red]in[/COLOR].enc ???&lt;BR /&gt;Those things matter on linux - file names are case sensitive.&lt;BR /&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Point taken, I appreciate the case sensitivity of Linux.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: &lt;/STRONG&gt;&lt;BR /&gt;&lt;BR /&gt;Again, part marked red is a group. It is clearly seen that its not plugdev but root&lt;BR /&gt;Which means - you have messed something with udev rules, which means again, you as a member of plugdev has no right to write to the device and here is your permission issue.&lt;BR /&gt;&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm not sure how this was caused. I did modify the group settings for plugdev (added myself to it, but there's no reason it should have showed up as root)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: &lt;/STRONG&gt;&lt;BR /&gt;&lt;BR /&gt;The reason is:&lt;BR /&gt;you either copy/paste the code that i gave, or edit with your editor, but!!!! remove the backslashes from quotes, which means, if you see '[COLOR=red]\"[/COLOR]' and edit the rules file with the editor you should replace it with '[COLOR=red]"[/COLOR]', or simplier copy/paste my input (this is the real shortcut lol)&lt;BR /&gt;&lt;BR /&gt;Try again, fixing the issues i pointed out.&lt;BR /&gt;&lt;BR /&gt;If you still want to use the gedit, put this into rules file:&amp;nbsp; 80-lpcxpresso.rules&lt;BR /&gt;&lt;TABLE border="1"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD bgcolor="#cacaca"&gt; &lt;PRE&gt;
# Rules for LPCXpresso DevBoard
SUBSYSTEM=="usb", ATTRS{idVendor}=="0471", ATTRS{idProduct}=="df55", MODE="0664", GROUP="plugdev"
SUBSYSTEM=="usb", ATTRS{idVendor}=="1fc9", ATTRS{idProduct}=="0009", MODE="0664", GROUP="plugdev"
&lt;/PRE&gt; &lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Again point taken, when I created the file using gedit I did take care to remove the unnecessary parts. The file was exactly as in your post.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: &lt;/STRONG&gt;&lt;BR /&gt;&lt;BR /&gt;and dont forget to restart udev&lt;BR /&gt;&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Did that as you specified.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: &lt;/STRONG&gt;&lt;BR /&gt;&lt;BR /&gt;PS.&lt;BR /&gt;The reason i wrote the commands i wrote in the previous post is to really give you a way to use console and not to rely on ubuntu gui.&lt;BR /&gt;Console is power. Do not rely on the gui. Read howtos and learn basic commands, this is linux after all, not windows.&amp;nbsp; This is one of the things that annoys me in UBUNTU.&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I appreciate your patience with someone not very familiar with Linux, I do come from a point-and-click background, but my command line skills are improving. I am also mid project and under pressure, the dev tool was giving me problems and therefore took the short cut. Some of the command line strings you sent me are quite long and typos can cause unforeseen errors as we see above.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Okay, now regarding feedback on current status; you may be able to understand what is taking place from events next.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I was encountering the code size limit error in debug as mentioned by other&amp;nbsp; users. I un-installed LPCXpresso completely and reinstalled it, generated a new serial number and activation code, after which the code size errors were removed. However, I did notice that debug had started working again as a normal user.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;At this point I needed to checkin some code to our svn repository, not having a suitable client I installed RapidSVN (via Ubuntu's software centre) and returned to LPCXpresso to continue working. At this point I found debug had quit operating and returned to its old behaviour.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Suspecting the installation of the new application had upset something, I un-installed LPCXpresso completely and reinstalled it as before. Again debug started working properly. To verify I did a complete system reboot and debug continued working.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm not sure how installing new software is handled by Ubuntu and its affects on LPCXpresso debug settings which seems to cause this trouble. As I had mentioned earlier it always worked the first time after installation, but since this is a new OS installation I had been adding other applications needed along the way. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm not saying this is the problem, but this is my observation at present.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks again for all the assistance.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;malcolm&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;PS: I did try the suggestion of the new rules file made by CodeRed support. But have removed it since and things are fine.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:59:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC-Link-connection-problems/m-p/568726#M19384</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T00:59:45Z</dc:date>
    </item>
    <item>
      <title>Re: LPC-Link connection problems</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC-Link-connection-problems/m-p/568727#M19385</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by TheFallGuy on Fri May 04 03:17:22 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: &lt;/STRONG&gt;&lt;BR /&gt;&lt;BR /&gt;At this point I needed to checkin some code to our svn repository, not&amp;nbsp; having a suitable client I installed RapidSVN (via Ubuntu's software&amp;nbsp; centre) and returned to LPCXpresso to continue working.&lt;BR /&gt;&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Did you know that you can add Subversion directly into LPCXpresso, by installing the Subclipse plugin?&lt;/SPAN&gt;&lt;BR /&gt;&lt;A href="http://"&gt;http://support.code-red-tech.com/CodeRedWiki/VersionControl&lt;/A&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:59:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC-Link-connection-problems/m-p/568727#M19385</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T00:59:45Z</dc:date>
    </item>
  </channel>
</rss>